Home Language Imprint Terms of Use www.bosch.com    
Bosch Rexroth
Language
english
deutsch
Bosch Rexroth Filtration Systems GmbH
About
News and Press
Events and Fairs
Products
Filter Program
Filter Elements
Filter Materials
Oil Purification
Measuring Instruments
Filter Accessories
Know-how
Why to use Filters?
Contamination
Oil Cleanliness Codes
Recommended Oil Cleanliness Codes for Components
Filter Parameters
Service
Industries
Jobs and Career
Training
Search Search   Contact Contact   Sitemap Sitemap  
image x  


Know-how

Oil Cleanliness Codes

The contamination level in hydraulic and lubricating oils is characterized by the so called oil cleanliness code.

Due to their shape, fit, dirt sensitivity, function and operating method different components tolerate different contamination levels of operating fluids. In order to meet this circumstance, by means of the contamination's particle distribution the contamination level of operating liquids is divided in different classifications, the so-called oil cleanliness codes.
The most frequently used classification for oil cleanliness codes in fluid power is defined by the international standard ISO 4406. Another important standard for oil cleanliness codes is represented by the SAE 4059 which replaces the recently valid NAS 1638.


Oil cleanliness codes as per ISO 4406
(excerpt from ISO 4406, issue 1999)

No. of particles > indicated size   
From To ISO Code 
64 130 
130 250 
250 500 
500 1.000 10 
1.000 2.000 11 
2.000 4.000 12 
4.000 8.000 13 
8.000 16.000 14 
16.000 32.000 15 
32.000 64.000 16 
64.000 130.000 17 
130.000 250.000 18 
250.000 500.000 19 
500.000 1.000.000 20 
1.000.000 2.000.000 21 
2.000.000 4.000.000 22 
4.000.000 8.000.000 23 



The classification of the cleanliness level

The oil cleanliness codes according to ISO 4406 may measured either by automatic or microscopically particle counting.


Automatic particle counting

The classification of the cleanliness level of an hydraulic oil consists usually out of an 3-digit code indicating the cleanliness code for particles > 4µm , > 6µm und > 14 µm

Example:
The oil sample taken from a hydraulic system was measured with an automatic particle counter.

The result of the particle count is as follows:

Particle size distribution in 100 ml oil  ISO Code 
92.350 Particles > 4 µm (c) 17 
17.812 Particle > 6 µm (c) 15 
1.219 Particle > 14 µm (c) 11 


Result: According to ISO 4406 this hydraulic oil has an oil cleanliness of: ISO 17 / 15 / 11.

If an automatic particle counter is used during the analysis of an oil sample the above mentioned 3-digit-code is used.


Microscopically particle counting:

Due to its condition an oil sample has to be counted in some cases using a light microscope. In that case a 2-digit-code is used only. This code belongs to all particles > 5µm and >15µm.

Example:
Particle size distribution in 100 ml Oil  ISO Code 
92.350 Particles > 5 µm 17 
17.812 Particles > 15 µm 15 


Oil cleanliness codes as per SAE AS 4059
(Excerpt)

As an alternative to the ISO 4406 the NAS 1638 was used up to now in fluid power.
This standard has now been replaced by the SAE standard AS 4059.
In contrary to the ISO 4406 this standard does not classify only the fine and silt particles but also coarse particles > 70 µm.

Maximum no. of particles for indicated cleanliness code in 100 ml sample.
       
Calibration NAS 1638 >1µm >5µm >15µm >25µm >50µm >100µm  
Calibration NAS SAE AS 4059 >4µm >6µm >14µm >21µm >38µm >70µm 
Range 
Code 0 780 304 54 10 
Code 1 1.560 609 109 20 
Code 2 3.120 1.220 217 39 
Code 3 6.520 2.430 432 76 13 
Code 4 12.500 4.860 864 152 26 
Code 5 25.000 9.730 1.730 306 53 
Code 6 50.000 19.500 3.460 612 106 16 
Code 7 100.000 38.900 6.920 1.220 212 32 
Code 8 200.000 77.900 13.900 2.450 424 64 
Code 9 400.000 156.000 27.700 4.900 848 128 
Code 10 800.000 311.000 55.400 9.800 1.700 256 
Code 11 1.600.000 623.000 111.000 19.600 3.390 512 
Code 12 3.200.000 1.250.000 222.000 39.200 6.780 1.024 



The complete standards of ISO 4406 resp. SAE 4059 are distributed through the relating organisations (ISO, SAE)