|
Product Information
[PI 017-09] |
 |
[10.02.09] |
Rexroth IndraMotion for Packaging: Machinery and Robot Functions in Combination |
 |
|
|
Cama places the compact MN robot alongside the mac |
|
 |
By combining Motion, Logic and Robotics in IndraMotion for Packaging, the system solution with multi-kinematics capability, Rexroth makes it easier to integrate robots in fully automatic plants. The control system operates up to 16 kinematic chains, each with a maximum of 8 interpolating axes for positioning, orientation and belt drive. In this way the Italian Cama Group greatly reduces the automation effort for integrating a variety of its own robot families in secondary packing plants.

Cama uses the multi-kinematics capability of IndraMotion for Packaging for the efficient and speedy integration of one or more robots. The control system covers all plant layouts from the stand-alone machine to the fully automatic packing line, thus accelerating the project planning and commissioning.

Both the newly developed MN-530 2-axis robot and the high-end Triaflex delta robot with four controlled axes are integrated by Cama without an additional robot control system. The new, cost-effective MN-530 robot uses an up to 600 mm wide pick-up tool to move loads of up to 15 kg at a product-dependent rate of 65 cycles per minute. The Italian manufacturer places the compact MN robot alongside the machine frame, thus saving the high expense of a ceiling-fitted arrangement.

The machine control cabinet accommodates the entire power electronics for all Cama robot families in minimum space. This reduces not only the amount of installation space required but also the amount of cabling work. IndraWorks, the standardized engineering software from Rexroth, makes it easier for Cama to program its own kinematic chains. SERCOS III, the internationally standardized Ethernet-based real-time system for control communication, provides greater freedom where complex plants are concerned. The Cama Group can interlink and synchronize any number of axes using the real-time cross-communication between several controller-based Rexroth control systems.

The system solution enables the simple integration of camera systems and the straight-forward retrofitting of robots in existing plants.
Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving machinery used in industrial and factory automation as well as in mobile applications. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2007 Bosch Rexroth AG, part of the Bosch Group, achieved sales of about 5.4 billion Euro with approximately 33,000 employees.


Reader Inquiries:

Tel.: +49 9352 40-4552
Fax: +49 9352 403-4552
E-Mail: susanne.herzlieb@boschrexroth.de
Adress: P.O. Box 1357, D-97803 Lohr a. Main
|
|
 |
|
 |
|
|
|
|