Home Language Imprint Terms of Use www.bosch.com    
Bosch Rexroth
Bosch Rexroth AG
Products and Solutions
Products
Industries
Trends and Topics
Customer Service
Training
How to buy
Company
About Rexroth
Trade Shows and Events
Press
The Company
Press Releases
Corporate Information
Product Information
Photo-News
Press Archive
Industry Trends and Statement Services
Press Kits
Contact
Jobs and Career
Procurement
Contact
Search Search   Contact Contact   Sitemap Sitemap  
image x  

Product Information

[PI 111-09]

[05.10.09]

EMO 2009

Rexroth Boosts Energy Efficiency through Machine Tool Automation
Systematic approach across all automation technologies

Rexroth 4EE — Rexroth for Energy Efficiency: A four-pronged cross-technology approach for increased energy efficiency.
Systematic approach across all automation technologies

Machine tools equipped with automation solutions from Rexroth consume almost 50% less energy while still maintaining the same high level of productivity. The drive and control technology manufacturer consistently uses the Rexroth 4EE concepts to boost energy efficiency throughout the machine's service life — from the engineering stage to day-to-day operation. This significantly reduces operating costs and therefore costs per unit over the machine's entire useful life.

The strategy is based on energy-efficient components such as optimized servomotors and switch valves featuring an energy-saving mode. In addition, lightweight linear components such as the new slimline roller runner blocks reduce the total mass to be moved, thereby lowering the amount of drive power required. Rexroth offers machine manufacturers a comprehensive mechatronics support service to help them select and dimension the various automation components and identify potential areas for savings. The groundbreaking new IndraMotion MTX cta (cycle time analyzer) and MTX ega (energy analyzer) analysis tools allow the user to accurately record a machine tool's duration of movement and energy consumption online during operation. When integrated into Rexroth system solutions, these tools show NC programmers how they can save energy through optimized motion control, while still maintaining a short cycle time. Rexroth Service supports manufacturers in performing in-depth data analysis and can also assist with system optimization on request.

Consistently using Energy on Demand to regulate accessory drive requirements forms another cornerstone of the strategy. Rexroth Blue Hydraulic Drives, a scalable range of variable-speed pump drives, cut existing energy requirements for hydraulic systems by between 40 and 70 percent. The hydraulic modulators from Rexroth work together with the newly unveiled cooling lubricant booster to provide compressed air to the cooling lubricant system. This revolutionary new concept does away with the need for a second power train with its own energy requirements, leading to energy and cost savings while maintaining a high level of machine tool robustness. The new VT-ZBUS bus module uses innovative pulse width modulation to ensure demand-driven energy consumption on switch valves, thereby achieving energy savings of up to 66 percent and increased service life of the switch solenoids.

The modular IndraDrive drive controllers use carefully dimensioned DC buses to simplify the use of braking energy. Consistent use of the various Rexroth 4EE concepts yields energy savings of up to 45 percent on cutting machine tools, while maintaining the same high level of productivity.

Rexroth at the EMO 2009 in Hall 3, Stand G18/H27



Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving. Bosch Rexroth is a partner for industrial applications and factory automation, mobile applications and using renewable energies. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2008 Bosch Rexroth AG, part of the Bosch Group, achieved sales of around 5.9 billion Euro with 35,300 employees.

For more information please visit: www.boschrexroth.com




Contact for Journalists:

Bosch Rexroth AG
Chantal van Mierlo
Maria-Theresien-Str. 23, 97816 Lohr
Phone: +49 9352 18-1573
Fax: +49 9352 18-1802
chantal.vanmierlo@boschrexroth.de
Downloads
Text (*pdf)
Image (*jpg)
 
 
go to top of page | Print | Create PDF