|
|
|
|

|
Product Information
[PI 110-09] |
 |
[21.09.09] |
Specialists Combine Automation Expertise for the Solar Industry |
 |
|
|
A sample module production line, typical for the majority of solar plants. |
|
 |
Rexroth Solar Team Uses Global Service and Development Resources

Bosch Rexroth is continuing to press ahead with the focus on tailor-made automation solutions for the solar industry: In a strong team, specialists combine application expertise on electrical, mechanical and pneumatic drive technology. The team supports machine manufacturers and users with comprehensive automation advice and innovative solutions for drive and control technology. The specialists have direct access to the international development capacity at Rexroth.

Here the experts draw on the comprehensive automation range from Rexroth, which already comprises a whole host of products and solutions specially developed for use in the solar industry. The possibility to combine pneumatic and electro-mechanical actuators with form-locking fixing technology increases the flexibility of tailor-made handling solutions for all production steps. In terms of controls, Bosch Rexroth combines PLC, motion and robotic functions in a single hardware system while consistently using open interfaces and applying programming standards such as the IEC 61131. This enables the economic standardization of global production associations where automation is concerned — even when the system is used in combination with architectures that differ by region.

Solutions optimized for energy efficiency cut production costs for solar modules on a permanent basis. Innovative products and requirement regulations are alone responsible or reducing energy consumption by up to 55% in the pneumatics sector. The continuous reuse of braking energy and the reduction in weight of linear technology has also lowered the power requirements of electrical drive technology to the same degree. Careful handling of movement patterns and contact-free grippers optimized for solar cells protects the cells against damage. Large and sensitive solar modules are transported on the Rexroth TS 2pv transfer system. A further contribution toward increasing productivity are the drive internal safety functions, which reduce the amount of time spent restarting the machines after manual intervention and thus significantly increase the availability of production lines.

Rexroth at the PVSEC in Hall B2G, Stand 03

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving. Bosch Rexroth is a partner for industrial applications and factory automation, mobile applications and using renewable energies. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2008 Bosch Rexroth AG, part of the Bosch Group, achieved sales of around 5.9 billion Euro with 35,300 employees.

For more information please visit: www.boschrexroth.com


Contact for Journalists:

Bosch Rexroth AG
Chantal van Mierlo
Maria-Theresien-Str. 23, 97816 Lohr
Phone: +49 9352 18-1573
Fax: +49 9352 18-1812
chantal.vanmierlo@boschrexroth.de |
|
 |
|
 |
|
|
|
|
|
| |
| |
|
|
|