<?xml version="1.0" encoding="utf-8" ?>

<rss version="2.0">
<channel>


























						
				
<title>Rexroth Pneumatics</title><link>http://www.boschrexroth.com/corporate/en/company/press/press_releases/rss_feeds/brp/index.jsp</link><description>Product News</description><language>en</language><pubDate>Fri, 29 May 2009 11:24:52 CEST</pubDate><item><title>[PI 007-09] : A Compact Solution - Valve terminal system with integrated I/O link interface
</title><link>http://www.boschrexroth.com/corporate/en/company/press/press_releases/product_information/pneumatics/archive_2009/pi_007_09_IO_Link/index.jsp</link><description>Rexroth offers easier commissioning and maintenance as well as expanded diagnostic possibilities with the introduction of the I/O link interface in pneumatics. To support the new, open communication standards, the proven LS04 valve terminal system ...</description><pubDate>Fri, 16 Apr 2010 18:00:17 CEST</pubDate></item><item><title>[PI 125-09]  : High Performance for Small Areas
TC08 and TC15 valve series with 2x3/2 functions
</title><link>http://www.boschrexroth.com/corporate/en/company/press/press_releases/product_information/pneumatics/archive_2009/PI_125_09_tc_en/index.jsp</link><description>With new 2x3/2 versions for single valves and valve terminal systems, Rexroth offers even more functions and flexibility for its reliable and proven TC valve series. The new double 3/2-way functions, with a flow of 600 l/min for the TC08 line and 110...</description><pubDate>Tue, 17 Nov 2009 00:00:00 CET</pubDate></item><item><title>[PI 074-09] : Up to 55% Savings in Energy Costs with Rexroth Pneumatics!
Rexroth presents a highly efficient compressed air application as the key to success at the Fachpack trade fair
</title><link>http://www.boschrexroth.com/corporate/en/company/press/press_releases/product_information/pneumatics/archive_2009/pi_074_09_Energy_Efficiency_Fachpack/index.jsp</link><description>For Rexroth, the decisive factors for conserving compressed air are a reduction in hose lengths, demand-based pressure regulation, and the proper dimensioning of components. To ensure reliable machine operation, large compressed air reserves w...</description><pubDate>Tue, 29 Sep 2009 00:00:00 CEST</pubDate></item><item><title>[PI 069-08]  : PVSEC 2009
Gentle Transport 
Contactless transfer of solar cells in production
</title><link>http://www.boschrexroth.com/corporate/en/company/press/press_releases/product_information/pneumatics/archive_2009/PI_069_08_en/index.jsp</link><description>The production of solar cells involves highly sensitive workpieces, since classical solar cells are just a few millimeters thick. The NCT transport units from Rexroth lift and move these highly sensitive workpieces gently. Even difficult-to-handle...</description><pubDate>Mon, 21 Sep 2009 00:00:00 CEST</pubDate></item><item><title>[PI 073-09] : Save Up to 55% in Energy Costs with Pneumatics from Rexroth!
Rexroth presents a highly efficient compressed air application as the key to success at the drinktec trade fair

</title><link>http://www.boschrexroth.com/corporate/en/company/press/press_releases/product_information/pneumatics/archive_2009/pi_073_09_Energy_Efficiency_drinktec/index.jsp</link><description>For Rexroth, the decisive factors for conserving compressed air are proper dimensioning of components, a reduction in hose lengths, and targeted pressure regulation. Furthermore, changes caused by wear can be detected at an early stage using condit...</description><pubDate>Mon, 14 Sep 2009 00:00:00 CEST</pubDate></item><item><title>[PI 073-09] : “Future-proof with Highly Efficient Systems”
Pneumatic solutions from Rexroth save energy costs of up to 55% delivering highest reliability

</title><link>http://www.boschrexroth.com/corporate/en/company/press/press_releases/product_information/pneumatics/archive_2009/pi_072_09_Statement_Vorbericht_drinktec/index.jsp</link><description>Intelligently linked measures are applied to make considerable energy savings. Rexroth has developed a strategy for a sustainable efficiency increase throughout the machine's service life. For pneumatic applications, the main factors include avoid...</description><pubDate>Fri, 24 Jul 2009 00:00:00 CEST</pubDate></item><item><title>[PI 109-06] : Marex OS II – the innovative ship remote control from Rexroth</title><link>http://www.boschrexroth.com/corporate/en/company/press/press_releases/product_information/pneumatics/archiv_2006/pi_109_06_marex/index.jsp</link><description>Marex OS II – the latest generation of electronic remote control systems for ship propulsions stands for the consequential advancement and extension of the product range. The latest extension, the control head type 244 offers modern design and new ...</description><pubDate>Fri, 17 Jul 2009 11:11:47 CEST</pubDate></item><item><title>[PI 008-09] : Protection against confusion and product piracy - Rexroth presents its new process for indentifying valves in valve terminal systems
</title><link>http://www.boschrexroth.com/corporate/en/company/press/press_releases/product_information/pneumatics/archiv_2008/pi_008_09_RFID_en/index.jsp</link><description>At the HANNOVER MESSE (Hannover Fair) 2009, Rexroth will present a new process for identifying valves on valve terminal systems that is based on RFID (Radio Frequence IDentification) technology. In doing so, Rexroth sets a new security standard tha...</description><pubDate>Tue, 17 Mar 2009 00:00:00 CET</pubDate></item><item><title>[PI 006-09] : Versatile and efficient - The new pneumatic valve terminal system from Rexroth
</title><link>http://www.boschrexroth.com/corporate/en/company/press/press_releases/product_information/pneumatics/archive_2009/PI_006_09_CD01_02_PI_en/index.jsp</link><description>Rexroth's CD01/02-PI pneumatic valve terminal system offers the greatest flexibility at a high level of standardization. Thanks to its modular and sturdy design, the valve terminal system offers the right solution for all application and control en...</description><pubDate>Tue, 17 Mar 2009 00:00:00 CET</pubDate></item><item><title>[PI 001-09] : More Flexibility with Compact Valves - Rexroth expands the functions of the HF04 pneumatic valve serie
</title><link>http://www.boschrexroth.com/corporate/en/company/press/press_releases/product_information/pneumatics/archive_2009/pi_001_09_HF04-XF_en/index.jsp</link><description>Rexroth introduces the HF04-XF (extended functionality) valve terminal system. The valve terminal system with extended functions has new base plates through which it can control up to 32 valve coils. The rotatable connection piece on the subbase en...</description><pubDate>Tue, 17 Mar 2009 00:00:00 CET</pubDate></item>
		</channel>
	</rss>