|
|
Product Information
[PI 014-08]
|
|
|
[04/21/2008] |
|
eLINE Guide Rails with Corrosion-resistant Steel Inserts in Accordance with DIN EN 10088
|
|
|
|
|
|
eLINE guide rails with corrosion-resistant steel inserts in accordance with DIN EN 10088 in combination with eLINE roller runner blocks.
|
|
|
The guide rails in Rexroth’s eLINE profiled rail systems are now also available with corrosion-resistant steel inserts. They therefore now make it possible, especially when combined with eLINE roller runner blocks, to create applications which are completely protected against corrosion, as required in certain areas of the medical technology sector, the food industry and the electronics industry. The load capacity remains just as high in spite of the corrosion-resistant material used for the ball tracks in the guide rails. The extra cost is in the region of just 5 percent for a single linear motion system comprised of two runner blocks on a one meter guide rail.

Rexroth developed the eLINE range of rail systems for applications associated with the manufacture of light-weight machinery and for plants and devices used for simple handling and assembly work, or in peripheral machine equipment and transportation solutions. Here it is economical realization in combination with high loading capacity that counts, with requirements and rigidity being only of secondary importance.

The runner blocks and guide rails are light weight, highly resistant to corrosion and of compact design while offering the same load capacity in all four principal load directions. A special feature is that it is possible to use two different roller element systems on a single rail - ball runner blocks and roller runner blocks. The extended interchangeability with the same connection dimensions makes logistics much simpler because the components can be ordered individually, and also increases design flexibility. This is also helped by the range of available accessories such as the clamping elements, for example, which are available for all three sizes. For special applications the facing surfaces on the guide rails can be delivered complete with a special black coating in order to further reduce the glare effect in optical testing or measuring equipment, for example. And with rollers on guide journals, individually available separately, the user can build his own mobile table with integrated guides himself.


Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving machinery used in industrial and factory automation as well as in mobile applications. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2006 Bosch Rexroth AG, part of the Bosch Group, achieved sales of approximately 4.9 billion Euro with more than 29,800 employees.

For more information please visit: www.boschrexroth.com


Contact for Journalists:

Bosch Rexroth AG
Dr. Wiebke Wittschen
Maria-Theresien-Str. 23, 97816 Lohr
Phone: +49 9352 18-1573
Fax: +49 9352 18-1802
wiebke.wittschen@boschrexroth.de


For product specific questions and reader inquiries:

Bosch Rexroth AG
Ingrid Alter
Postfach 30 02 07, 70442 Stuttgart
Phone: +49 711 811-46181
Fax: +49 711 811-31543
ingrid.alter@boschrexroth.de

|
|
|
|
|
|
|
|