image x image x
Image trenn Image trenn  
    image x
image x image ximage x Linear Motion and Assembly TechnologiesPneumaticsService AutomationMobile Hydraulics Bosch Rexroth image x
image x
www.bosch.com
www.boschrexroth.com
Bosch Rexroth AG
About us
Press
The Company
Press Releases
Corporate Information
Product Information
Press Archive
Industry Trends and Statement Services
Press Kits
Press Images
Contact
Events and Trade shows
Products and Solutions
Industries
Customer Service
Training
Procurement
Bosch Rexroth worldwide
Jobs and Career
image x
image x
Search Search   Contact Contact   Addresses Addresses   Sitemap Sitemap   image x image x image x image x
image x

Product Information

[PI 015-08]

[04/21/2008]

Miniature Ball Rail Systems for Even Higher Loads

 
Rexroth miniature ball rails systems with runner blocks in wide and long versions.
Rexroth has expanded its range of miniature ball rail system products by adding long versions of the wide runner blocks to supplement the standard length versions. They are the optimum solution for applications involving the kinds of higher loads associated with automation and handling, for example, where smooth running is essential, and are absolutely ideal for single-rail applications involving two or even just one runner block.

The new wide and long runner blocks have a 40 percent higher dynamic load capacity and 100 percent higher torque capacity compared to previous standard length runner blocks. Like all of Rexroth’s miniature ball rail systems these runner blocks are designed for speeds of up to 3 m/s and accelerations of up to 250 m/s².

In combination with single-piece guide rails, which Rexroth supplies for all sizes up to 2000 millimeters in length, they can be used to achieve new structural solutions at very low cost. The guide rails are also available, as before, as multi-piece versions as well of course.

The rails can also be supplied with the fixing holes sealed with a non-corrosive cover strip, which is available as an option. This eliminates the need for the effort involved in sealing the holes with plastic plugs and also provides a more effective seal while looking better at the same time.

For an overview of the comprehensive range of miniature ball rail system products, please refer to catalog R310EN2210.




Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving machinery used in industrial and factory automation as well as in mobile applications. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2006 Bosch Rexroth AG, part of the Bosch Group, achieved sales of approximately 4.9 billion Euro with more than 29,800 employees.

For more information please visit: www.boschrexroth.com




Contact for Journalists:

Bosch Rexroth AG
Dr. Wiebke Wittschen
Maria-Theresien-Str. 23, 97816 Lohr
Phone: +49 9352 18-1573
Fax: +49 9352 18-1802
wiebke.wittschen@boschrexroth.de



For product specific questions and reader inquiries:


Bosch Rexroth AG
Ingrid Alter
Postfach 30 02 07, 70442 Stuttgart
Phone: +49 711 811-46181
Fax: +49 711 811-31543
ingrid.alter@boschrexroth.de


image x
image x Keyword Search image x
image x
image x image x
image x Search image x
image x
image x Downloads image x
image x
image x image x Text (*pdf, 45 KB) image x
image x image x Image (*jpg, 804 KB) image x
image x
image x
 
 
go to top of page | Print