image x image x
Image trenn Image trenn  
    image x
image x image ximage x Linear Motion and Assembly TechnologiesPneumaticsService AutomationMobile Hydraulics Bosch Rexroth image x
image x
www.bosch.com
www.boschrexroth.com
Bosch Rexroth AG
About us
Press
The Company
Press Releases
Corporate Information
Product Information
Press Archive
Industry Trends and Statement Services
Press Kits
Press Images
Contact
Events and Trade shows
Products and Solutions
Industries
Customer Service
Training
Procurement
Bosch Rexroth worldwide
Jobs and Career
image x
image x
Search Search   Contact Contact   Addresses Addresses   Sitemap Sitemap   image x image x image x image x
image x

Product Information

[PI 058-08]

[04/29/2008]

AUTOMATICA 2008

Rexroth's TSsolar Transfer System for Safe and Clean Transport of Highly-Sensitive Photovoltaic Modules

 
Rexroth's TSsolar transfer system for transporting photovoltaic modules
Photovoltaic modules in thin-film and silicon cell technology can be transported directly on the new Rexroth TSsolar transfer system. The TSsolar is based on the proven TS 2plus transfer technology and has been customized to suit the specific demands in the solar industry.

It is ideal for standardized series production with high-volume, top-quality output. Thanks to their closed surface and a special treatment, the system’s toothed belts feature particularly low friction and wear. The TSsolar fulfills the requirements for clean room class 6 (DIN EN ISO 14644-1) and can be used throughout ESD environments. As accumulation of solar components is not permitted during transport, each section element has its own drive. Frequency converters enable the soft stop and accelerating operations required for the sensitive solar products.

Depending on the module size, users can select from various conveyor sections with multiple tracks and lengths of up to six meters. Rexroth also offers the right lift transverse units to move the products from longitudinal to transverse conveyors. A special heat-resistant conveyor version is available for applications such as transporting hot glass plates with temperatures of up to 200°C.

As with all of Rexroth's other transfer systems, the pre-assembled and ready-to-use TSsolar components can be freely combined with elements from the Manual Production Systems range and modular aluminum profile system.

Rexroth will be exhibiting at the 2008 Automatica in hall A1, stand 103.




Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving machinery used in industrial and factory automation as well as in mobile applications. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2007 Bosch Rexroth AG, part of the Bosch Group, achieved sales of about 5.4 billion Euro with approximately 33,000 employees.

For more information please visit: www.boschrexroth.com




Contact for Journalists:

Bosch Rexroth AG
Dr. Wiebke Wittschen
Maria-Theresien-Str. 23, 97816 Lohr
Phone: +49 9352 18-1573
Fax: +49 9352 18-1802
wiebke.wittschen@boschrexroth.de



For product specific questions and reader inquiries:


Bosch Rexroth AG
Ingrid Alter
Postfach 30 02 07, 70442 Stuttgart
Phone: +49 711 811-46181
Fax: +49 711 811-31543
ingrid.alter@boschrexroth.de


image x
image x Keyword Search image x
image x
image x image x
image x Search image x
image x
image x Downloads image x
image x
image x image x Text (*pdf, 52 KB) image x
image x image x Image (*jpg, 890 KB) image x
image x
image x
 
 
go to top of page | Print