image x image x
Image trenn Image trenn  
    image x
image x image ximage x Linear Motion and Assembly TechnologiesPneumaticsService AutomationMobile Hydraulics Bosch Rexroth image x
image x
www.bosch.com
www.boschrexroth.com
Bosch Rexroth AG
About us
Press
The Company
Press Kits
Press Releases
Corporate Information
Product Information
Press Archive
Industry Trends and Statement Services
Contact
Press Images
Events and Trade shows
Products and Solutions
Industries
Customer Service
Training
Procurement
Bosch Rexroth worldwide
image x
image x
Search Search   Contact Contact   Addresses Addresses   Sitemap Sitemap   image x image x image x image x
image x

Product Information

[PI 079-08]

[07/16/2008]

MOTEK 2008

Fully Assembled Linear Guides from Rexroth’s Basic Mechanical Elements

 
Rexroth now offers linear guides from the basic mechanical elements (MGE) assembly system in three sizes and two versions, fully assembled.
Rexroth now offers linear guides from the basic mechanical elements (MGE) assembly system in three sizes and two versions, fully assembled. This saves the user planning effort and assembly time. New accessory parts complete the product range. In particular, the MGE linear guides fulfill the needs of simple handling and positioning movements. They can also be easily integrated in the frame, peripheral machine units, or transport solutions. Stainless steel guide rods give the products a sturdy backbone, enabling them to be used in challenging environments for loads from 85 to 600 kg.

The user can select two MSK servomotors for each size, according to load and speed, from the new range of accessories. Suitable flanges and drives round out the product range. There are ready-to-use sets for end position and positioning queries, available either as a mechanical or inductive switch, including support. The linear guides are fully assembled and with matching accessories, can be quickly integrated into other applications.

The revised MGE linear guide program provides a further customer benefit: Combinability with Rexroth’s eLINE system, thanks to the interface of the new eLINE slide profiles. The combination of the eLINE runner block, a screw connection and the tried and true MGE slot results in a user-friendly interaction.

Rexroth will be exhibiting at the Motek 2008 in hall 3, stand 3120.



Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving machinery used in industrial and factory automation as well as in mobile applications. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2007 Bosch Rexroth AG, part of the Bosch Group, achieved sales of about 5.4 billion Euro with approximately 33,000 employees.

For more information please visit: www.boschrexroth.com




Contact for Journalists:

Bosch Rexroth AG
Dr. Wiebke Wittschen
Maria-Theresien-Str. 23, 97816 Lohr
Phone: +49 9352 18-1573
Fax: +49 9352 18-1802
wiebke.wittschen@boschrexroth.de



For product specific questions and reader inquiries:


Bosch Rexroth AG
Ingrid Alter
Postfach 30 02 07, 70442 Stuttgart
Phone: +49 711 811-46181
Fax: +49 711 811-31543
ingrid.alter@boschrexroth.de


image x
image x Keyword Search image x
image x
image x image x
image x Search image x
image x
image x Downloads image x
image x
image x image x Text (*pdf, 43 KB) image x
image x image x Image (*jpg, 1.040 KB) image x
image x
image x
 
 
go to top of page