<?xml version="1.0" encoding="utf-8" ?>

<rss version="2.0">
<channel>


























						
				
<title>Rexroth Industrial Hydraulics</title><link>http://www.boschrexroth.com/corporate/en/press/press_releases/rss_feeds/bri/index.jsp</link><description>Product News</description><language>en</language><pubDate>Fri, 7 Mar 2008 13:31:04 MET</pubDate><item><title>[PI 143-08]  : Energy-Efficient Forming - Variable-speed Pump Drives from Rexroth
</title><link>http://www.boschrexroth.com/corporate/en/press/press_releases/product_information/bri_en/PI_143_08_en/index.jsp</link><description>Energy savings of up to 50 percent; up to 60 percent reduction in heat input for hydraulic oil and up to 15 decibels less noise: Rexroth offers long-term reductions in operating costs with variable-speed pump drives for forming technology. Ready-t...</description><pubDate>Tue, 21 Oct 2008 00:00:00 MEST</pubDate></item><item><title>[PI 144-08]  : Simple, Complete, Efficient - Highly Dynamic Cylinder Axis from Rexroth
</title><link>http://www.boschrexroth.com/corporate/en/press/press_releases/product_information/bri_en/PI_144_08_en/index.jsp</link><description>Tailored to suit each application and ready to install, electrohydraulic axes from Rexroth simplify the automation of machine tools. The complete system solutions include all the necessary hardware and software components for various different mac...</description><pubDate>Tue, 21 Oct 2008 00:00:00 MEST</pubDate></item><item><title>[PI 150-08]  : The Rexroth Online Platform for Repairs - Fast Processing 24 Hours a Day
</title><link>http://www.boschrexroth.com/corporate/en/press/press_releases/product_information/bri_en/PI_150_08_en/index.jsp</link><description>With the online service for repairs, Rexroth simplifies and accelerates the order granting, decision-making and processing for the repair of hydraulic components. Via the Internet, the user can at the same time always find out the current order st...</description><pubDate>Tue, 14 Oct 2008 00:00:00 MEST</pubDate></item><item><title>[PI 149-08]  : AZP+ Extra Service for External Gear Pumps 
from Rexroth - Fast Replacement for High Availability 
</title><link>http://www.boschrexroth.com/corporate/en/press/press_releases/product_information/bri_en/PI_149_08_en/index.jsp</link><description>With the AZP+ range from stock, Rexroth reduces production interruptions that have been caused by service cases in external gear pumps. An extensive selection of prefabricated assemblies, already assembled replacement part sets and numerous pump t...</description><pubDate>Tue, 14 Oct 2008 00:00:00 MEST</pubDate></item><item><title>[PI 134-08]  : Failsafe Power Solution Increases Availability of Wind Power Systems - Electrical Pitch Adjustment from Rexroth
</title><link>http://www.boschrexroth.com/corporate/en/press/press_releases/product_information/bri_en/PI_134_08_en/index.jsp</link><description>With an innovative system solution for electrical blade pitch adjustment, Rexroth is putting an end to the complete shut down of wind power systems, even in the event of small faults. Through two-way monitoring and a redundant system structure, if...</description><pubDate>Tue, 9 Sep 2008 00:00:00 MEST</pubDate></item><item><title>[PI 065-08]  : Pilot Operated Pressure Cut-Off Valve KAV by Rexroth  - 
Switching pressure differentials now continuously variable from 8 to 50 percent
</title><link>http://www.boschrexroth.com/corporate/en/press/press_releases/product_information/bri_en/PI_065_08_en/index.jsp</link><description>Rexroth guarantees more than 10 million cycles for the new pilot-operated pressure cut-off valve with mechanical actuation KAV 2.2AA/AV. Due to the freely adjustable switch-on and cut-off pressure, the robust component can be used in a great numbe...</description><pubDate>Tue, 9 Sep 2008 00:00:00 MEST</pubDate></item><item><title>[PI 106-08]  : New Winch Drive from Rexroth -
Robust Technology for Maritime Application</title><link>http://www.boschrexroth.com/corporate/en/press/press_releases/product_information/bri_en/PI_106_08_en/index.jsp</link><description>Rexroth used its many years of experience in the automation of nautical winches for the development of the new WCB15 winch control block. For the new assembly the manufacturer exclusively uses standard components which have proven successful for m...</description><pubDate>Fri, 8 Aug 2008 00:00:00 MEST</pubDate></item><item><title>[PI 104-08]  : Rexroth Hydraulics for Two-Stroke Marine Diesel Engine - 
BR-FIVA valve for ideal fuel consumption and low emissions
</title><link>http://www.boschrexroth.com/corporate/en/press/press_releases/product_information/bri_en/PI_104_08_en/index.jsp</link><description>It is hard to imagine life nowadays without ships as a modern mode of transport. They fulfill many tasks and have to measure to the most stringent requirements. For the technical systems on board this means: No compromises. Reliability, robustness...</description><pubDate>Fri, 8 Aug 2008 00:00:00 MEST</pubDate></item><item><title>[PI 099-08]  : Generating Renewable Energy with Proven Technology-
Rexroth hydraulics concentrates solar energy at a point </title><link>http://www.boschrexroth.com/corporate/en/press/press_releases/product_information/bri_en/PI_099_08_en/index.jsp</link><description>Rexroth equips reliable hydraulic tracking systems in solar power plants to increase output. The company sells its robust and highly sensitive solar tracking systems to leading manufacturers of solar thermal plants around the world. Like magn...</description><pubDate>Fri, 1 Aug 2008 00:00:00 MEST</pubDate></item><item><title>[PI 061-08]  : Dynamic and precise - Scalable Motion Controls from Rexroth for Printing and Converting Machines
</title><link>http://www.boschrexroth.com/corporate/en/press/press_releases/product_information/bri_en/PI_061_08_en/index.jsp</link><description>For the automation of printing and converting machines Rexroth works on optimized mechatronic components, which are fast and efficient. Rexroth opens up new degrees of freedom in the field of automation with a comprehensive portfolio of intelligen...</description><pubDate>Thu, 29 May 2008 00:00:00 MEST</pubDate></item>
		</channel>
	</rss>