Home Language Imprint Terms of Use www.bosch.com  1-800 REXROTH  
Bosch Rexroth
USA
Products and Solutions
Products
Industries
Trends and Topics
Documentation and Resources
Service
Training
How to Buy
Company
About Bosch Rexroth
Press
Company Overview
Press Releases
Corporate News
Multiple Technology
Electric Drives and Controls
Industrial Hydraulics
Mobile Hydraulics
Linear Motion and Assembly Technologies
Pneumatics
Press Archive
Rexroth Image Library
Trade Show Press Kits
What's New
Trade Shows and Events
Jobs and Careers
Contact Us
  Contact Contact   Sitemap Sitemap  
image x  

Product News: Electric Drives and Controls

[27.10.10]

PACK EXPO 2010: High-Performance MLC Version 10 Motion Logic and Robotics Controller with Flex Profile from Bosch Rexroth

Rexroth IndraControl L65 PAC for Motion Logic, Robotics with Flex Profile Camming.
(Hoffman Estates, IL – www.boschrexroth-us.com/brc) The Rexroth MLC motion logic controller with Version 10 firmware is based on a powerful one-gigahertz PAC controls platform that provides high-performance motion logic and robotics capabilities.

Rexroth’s most advanced platform supports real-time Ethernet communication on Ethernet platforms, including SERCOS III, Ethernet IP and ProfiNet for interfacing with connecting controls, drives, I/Os, safety, HMI, web and machine-to-machine synchronization, which helps to lower the controls cost and simplify integration for OEMs, systems integrators and end users.

The MLC motion control, Version 10, has Web-based Service & Engineering Tool for easy access using a web browser to access the system data, and also has configuration tools for maintenance and commissioning. The system status and diagnosis of control hardware, drives and communication interfaces can all be viewed. Also, available is the parameter editor, PLC variables, and electronic name plate data.

It uses IndraLogic 2nd Generation (2G) PLC editor that offers the following extensions and enhancements:
Object orientated programming in project structure, new data types, new operators and variables. IndraLogic 2G supports standard IEC 61131-3 program languages such as: Function Block Diagrams (FBD), Ladder Diagrams (LD), Instruction Lists (IL), Sequential Function Chart (SFC), and Structured Text (ST). It offers a new visualization concept for testing and monitoring functions as well as many more additional features.

Suitable for the most sophisticated packaging and high-speed robotics applications. The Rexroth MLC powerful processor allows for control of up to 32 robotic kinematics concurrently, and up to 64 axes of motion and logic on a single controller. The latest Version 10 firmware also provides advanced Flex Profile camming capabilities to help reduce engineering time and provide automatic cycle time optimization of machines and entire packaging lines.

With Flex Profile, cams can be multi-segmented and cycle times can be automatically optimized for velocity, acceleration, position or time to avoid having to rebuild cams each time a parameter changes. Provides masters as an axis, as a specific time, or a combination of both. By changing values in the segments the profile can be easily modified to accommodate any changes in products. With the MLC 10 Flex Profile can now generate PLC function blocks for online creation of FlexProfiles, CAM preview with several axes simultaneously and provide definition of FlexProfile events. Visit www.boschrexroth-us.com/BRC for more information.


Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving. Bosch Rexroth is a partner for industrial applications and factory automation, mobile applications and renewable energy. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2009 Bosch Rexroth, part of the Bosch Group, achieved sales of around $5.7 billion (4.1 billion Euro) with 34,200 employees.

For more information please visit: www.boschrexroth-us.com.



For more information, please contact:

Bosch Rexroth Corporation
Dan Throne
5150 Prairie Stone Parkway
Hoffman Estates, IL 60192
Telephone 1 (847) 645-3749
Fax (847) 645-6201
dan.throne@boschrexroth-us.com


Godfrey Public Relations
Todd Walter
40 North Christian Street
Lancaster, PA 17602
Telephone (717) 393-3831 ext. 133
Fax (717) 393-1403
twalter@godfrey.com
Downloads
Word Document (87.5 KB)
High-Resolution Image (1.1 MB)
Request Information
Use our online request form
 
 
go to top of page | Print | Create PDF