Home Language Imprint Terms of Use www.bosch.com  1-800 REXROTH  
Bosch Rexroth
USA
Products and Solutions
Products
Industries
Trends and Topics
Documentation and Resources
Service
Training
How to Buy
Company
About Bosch Rexroth
Press
Company Overview
Press Releases
Corporate News
Multiple Technology
Electric Drives and Controls
Industrial Hydraulics
Mobile Hydraulics
Linear Motion and Assembly Technologies
Pneumatics
Press Archive
Rexroth Image Library
Trade Show Press Kits
What's New
Trade Shows and Events
Jobs and Careers
Contact Us
  Contact Contact   Sitemap Sitemap  
image x  

Rexroth EasyHandling automates handling tasks economically, reduces engineering effort by up to 80 percent

[15.09.11]

AATExpo 2011: Rexroth EasyHandling automates handling tasks economically, reduces engineering effort by up to 80 percent

EasyHandling makes it possible to automate handling tasks economically, reducing engineering effort, and cost, by up to 80 percent
With its new mechatronics platform, Rexroth addresses the need for increasingly economic approaches to the automation of handling tasks. Systematic and seamless integration of all drive and control technologies with linear actuators, standardized mechanical and electrical interfaces, and new start-up and commissioning tools dramatically simplify the automation process. EasyHandling is more than just a modular system and reduces the total time required to assemble, configure and commission an installation by up to 80 percent.


(Charlotte, NC – www.boschrexroth-us.com) The Rexroth EasyHandling system solution is based on a three-level architecture, which includes basic, comfort, and advanced versions. These cover all levels of automation – from mechatronic actuators, to intelligent axes, through to complete preconfigured system solution.

The EasyHandling basic version spans all mechanical drive principles to create mechanical single- and multi-axis systems with motors and pneumatics, ready to install. Pneumatic actuators such as grippers and rotary modules, as well as sensors, are also available. An easy-to-use online selection tool shortens configuration and planning time.


Pre-configured servo drives, EasyWizard reduce effort further

The EasyHandling comfort level adds preconfigured Rexroth servo drives across the entire range of basic axes. Using newly developed hardware that supports several Ethernet protocols, servo drives realize communication with Rexroth IndraDrive Cs controllers via SERCOS III Ethernet, PROFINET IO, EtherNet/IP, and EtherCat. It is also possible to outfit the drives with a PROFIBUS or other traditional communication interface. The EasyHandling comfort version thus combines ultra-high versatility with unsurpassed ease in commissioning and start-up.

EasyWizard from Rexroth is a servo system commissioning tool in which specific electrical and mechanical data are quickly defined for each axis. EasyWizard recognizes the electronic nameplate of the Rexroth IndraDyn motor and links the data to the mechanical parameters after the part number of the linear module is entered. This narrows the scope of commissioning to the identification of just a few application-specific parameters and cuts the time otherwise required by up to 90 percent.

EasyHandling also greatly simplifies design and assembly, since Rexroth’s perfectly-matched Easy-2-Combine connection system cuts up to 75% of the time and effort needed for custom fabrication of adapter components.


Adaptable Maintenance Instructions Extend Service Life

In the third version, EasyHandling advanced, a preconfigured motion-logic controller compliant with the IEC 61131-3 and PLC open standards is pre-integrated into the handling systems by Rexroth. Handling tasks that used to require extensive programming can now be configured extremely fast thanks to predefined functions and an included ready-made HMI solution. The controller assumes the coordinated point-to-point motions and smoothing and optimized handling paths for Cartesian systems. Based on the axis-specific mechanical data defined, the drive controller software also provides the operator with maintenance instructions that correspond to the specific run times and travel paths. That makes it easier to adhere to lubrication intervals, thereby increasing service life and reducing the risk of mechanical failure.

Visit Bosch Rexroth at AATExpo 2011 in Chicago’s McCormick Place, booth 1308.

For more information, please visit www.easy-handling.com.



Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue ($6.8 billion) in 2010. To learn more, please visit www.boschrexroth-us.com

The Bosch Group is a leading global supplier of technology and services. In the areas of automotive and industrial technology, consumer goods, and building technology, some 285,000 associates generated sales of 47.3 billion euros ($62.7 billion) in fiscal 2010. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in over 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent 3.8 billion euros for research and development in 2010, and applied for over 3,800 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Additional information can be accessed at www.bosch.com, www.bosch-press.com.




For more information, please contact
Bosch Rexroth Corporation
Susan Strauss
2315 City Line Road
Bethlehem, PA 18017
Telephone (610) 694-8352
Fax (610) 694-8266
susan.strauss@boschrexroth-us.com


Godfrey Public Relations
Todd Walter
40 North Christian Street
Lancaster, PA 17602
Telephone (717) 393-3831 ext. 133
Fax (717) 393-1403
twalter@godfrey.com
Downloads
Word Document (328 KB)
High-Resolution Image (1.7 MB)
Request Information
Use our online request form
 
 
go to top of page | Print | Create PDF