Home Language Imprint Terms of Use www.bosch.com  1-800 REXROTH  
Bosch Rexroth
USA
Products and Solutions
Products
Industries
Trends and Topics
Documentation and Resources
Service
Training
How to Buy
Company
About Bosch Rexroth
Press
Company Overview
Press Releases
Corporate News
Multiple Technology
Electric Drives and Controls
Industrial Hydraulics
Mobile Hydraulics
Linear Motion and Assembly Technologies
Pneumatics
Press Archive
Rexroth Image Library
Trade Show Press Kits
What's New
Trade Shows and Events
Jobs and Careers
Contact Us
  Contact Contact   Sitemap Sitemap  
image x  

Press Release: Linear Motion & Assembly

[18.05.12]

Fast and light for long movements: Rexroth's Omega Module linear motion system adds even more capability to the EasyHandling modular system

The new Omega Module moves low traveling mass quickly.
Feed units in machine tools, assembly lines and handling applications often require fast deep plunges into large workspaces. Combined with the increasingly fast cycle times of production machines, this places especially high demands on the axis mechanics in automated processes. Rexroth's new linear motion system, the "Omega Module", addresses this need by featuring a very low traveling mass so that top speeds can be reached. The belt drive is fixed to both ends of the main body and is looped around the drive shaft of the table part in the shape of the Greek letter "Ω", reducing the module's mass considerably compared to ball screw assemblies, thereby making it highly dynamic. By guiding the module's table part over ball rail systems, the module achieves a high degree of rigidity for precise movements.

The Omega Module linear motion system allows for higher dynamics over longer distances in feed units, thanks to the combination of its low traveling mass and fast belt drive. Because the drive is stationary, the linear system can be set up in any position in addition to being used as a vertical axis. A pneumatic clamping element maintains the position at standstill and also clamps hanging loads.

As a single axis system, the Omega Module comes with the necessary mechanical and electrical interfaces to fit with the modular Rexroth EasyHandling system. The system’s standard Easy-2-Combine form-fit connection method, can speed assembly and reduce up-front engineering time, even in multi-axis systems.. In addition, it simplifies the direct attachment of pneumatic grippers and rotary modules, or other end-of-arm tooling.

One of the special features of EasyHandling is that it allows for fast start-up. With the EasyWizard commissioning tool, only a handful of axis-specific data needs to be entered, which helps to reduce start-up timeto just a few minutes. As a single-axis system, the Omega Module is ideal for assembly and handling applications or in other automation tasks.

The Omega Module comes in three sizes to handle a variety of performance requirements. With a stationary main body, users can specify custom lengths up to 5,500 mm and choose from main bodies (frames) with widths of 55, 85 or 120 mm. This set-up allows for several carriages with their own drive to be operated independently from each other. Rexroth offers the linear motion system with matching drives, motors and controllers. In the largest size, the mechanics are designed for input torques up to 154Nm. With high acceleration speeds of up to 50m/s² and speeds of up to 5m/s, it opens up the door for reduced cycle times even for longer movements.

To learn more, please visit www.boschrexroth-us.com

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial.

Further information is available online at www.bosch.com and www.bosch-press.com.
Downloads
Word Document (728 KB)
High-Resolution Image (435 KB)
Request Information
Use our online request form
 
 
go to top of page | Print | Create PDF