|
Product News: Pneumatics
|
 |
[05.02.10] |
Rexroth Adds Sercos III and Ethernet/IP to Pneumatic Valve Fieldbus Protocol Support - ATX West 2010 |
 |
|
|
Rexroth valves like the Series HF04 shown above now support Sercos III and EtherNet/IP and have all connections on one plane. |
|
 |
Rexroth has expanded the offering of B-Design fieldbus components to include support for Sercos III and Ethernet/IP for valve systems Series HF03-LG, HF04 and CD01/02-PI.

(Lexington, KY — www.boschrexroth-us.com) Rexroth announces the expansion of B-Design fieldbus components to include support for Sercos III and Ethernet/IP for valve manifold systems Series HF03-LG, HF04, and CD01/02-PI. The valves include body sizes with 10, 15, 18 and 26mm widths. All electric, pneumatic, supply and exhaust connections are on one plane, enabling clean installation. Discrete output modules control up to 2 amps current draw per point, and modular expansion of discrete and solenoid outputs is possible.

The Sercos III version follows the standard platform as other Rexroth Bus Direct Control (BDC) protocols. Sercos III features up to 32 outputs per valve manifold and up to four valve manifolds can be controlled from one bus module.

The EtherNet/IP version follows the standard platform as other Rexroth bus Central Mount System (CMS) protocols. EtherNet/IP features up to 48 inputs per valve manifold in addition to solenoid and discrete outputs, and up to four valve manifolds can be controlled by one bus module. The standard module works with EtherNet/IP, Modbus TCP and TCP/IP protocols.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving machinery used in industrial and factory automation as well as in mobile applications. Bosch Rexroth is a partner for industrial applications, factory automation, mobile applications and renewable energy development. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2008 Bosch Rexroth AG, part of the Bosch Group, achieved sales of around $8.3 billion (5.9 billion Euro) with 35,300 employees. Visit www.boschrexroth-us.com for more information.

For more information, please contact

Bosch Rexroth Corporation
John Bridges
1953 Mercer Road
Lexington, KY 40511-1021
Telephone (859) 259-3852
Fax (859) 281-3491
john.bridges@boschrexroth-us.com

Godfrey Public Relations
Todd Walter
40 North Christian Street
Lancaster, PA 17602
Telephone (717) 393-3831 ext. 133
Fax (717) 393-1403
twalter@godfrey.com
|
|
 |
|
 |
|
|
|
|