Home Language Imprint Terms of Use www.bosch.com  1-800 REXROTH  
Bosch Rexroth
USA
Products and Solutions
Products
Industries
Trends and Topics
Documentation and Resources
Service
Training
How to Buy
Company
About Bosch Rexroth
Press
Company Overview
Press Releases
Corporate News
Multiple Technology
Electric Drives and Controls
Industrial Hydraulics
Mobile Hydraulics
Linear Motion and Assembly Technologies
Pneumatics
Press Archive
Rexroth Image Library
Trade Show Press Kits
What's New
Trade Shows and Events
Jobs and Careers
Contact Us
  Contact Contact   Sitemap Sitemap  
image x  

Press Releases: Pneumatics

[20.09.11]

AATExpo 2011: RTC Rodless Pneumatic Cylinders from Rexroth

Rexroth RTC rodless cylinders now available in lengths up to 23 feet with reduced lead time.
RTC rodless cylinders from Rexroth are ideal for powerful applications in tight installation conditions. The pneumatic cylinders are available in three versions, providing the right solution for every demand.

(Lexington, KY – www.boschrexroth-us.com/brp) The Rexroth RTC (Rodless Thrust Cylinder) line of pneumatic cylinders are now available from Lexington, KY in lengths up to 23 feet with two weeks lead time. Previously, shorter strokes (up to 118”) were already on the GoTo focused delivery program with a one week lead time. The RTC features a high load capacity, space saving design with speeds up to 22 feet per second.

Be it high precision, compact dimensions, high performance, or cost-effectiveness - the cylinders in the RTC series are available in three versions. While the basic version RTC-BV (Basic Version) is suitable for general use, the RTC-CG (Compact Guide) version offers high precision packed into compact dimensions. The RTC-HD (Heavy Duty) version is designed for handling heavy loads with precision.

The RTC is available in diameters of 16-80 mm (5/8”-3”) and with a maximum stroke length of 9900 mm (32.5 ft.), depending on version and size, and is available with ISO-G or NPT ports. Online configurator and calculation programs help determine the right cylinder for every application and CAD files can be downloaded.

An oval-shaped piston provides excellent load capacity and high moment resistance. The slide and piston in the RTC are constructed as a single unit allowing it to move higher loads than other cylinders. The RTC guided versions (RTC-CG and RTC-HD) come with an Easy-2-Combine interface allowing simple combination with many other Rexroth actuators and components.

The RTC is part of the Rexroth Easy Handling system which easily integrates controls, pneumatic and electro-mechanical actuators, plus aluminum framing into a system optimized for customers’ applications.


Visit Bosch Rexroth at AATExpo 2011 in Chicago’s McCormick Place, booth 1308. For more information, please visit www.boschrexroth-us.com/brp.



Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue ($6.8 billion) in 2010. To learn more, please visit www.boschrexroth-us.com.

The Bosch Group is a leading global supplier of technology and services. In the areas of automotive and industrial technology, consumer goods, and building technology, some 285,000 associates generated sales of 47.3 billion euros ($62.7 billion) in fiscal 2010. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in over 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent 3.8 billion euros for research and development in 2010, and applied for over 3,800 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Additional information can be accessed at www.bosch.com, www.bosch-press.com.



For more information, please contact

Bosch Rexroth Corporation
Susan Strauss
2315 City Line Road
Bethlehem, PA 18017
Telephone (610) 694-8352
Fax (610) 694-8266
susan.strauss@boschrexroth-us.com


Godfrey Public Relations
Todd Walter
40 North Christian Street
Lancaster, PA 17602
Telephone (717) 393-3831 ext. 133
Fax (717) 393-1403
twalter@godfrey.com
Downloads
Word Document (780 KB)
High-Res. Image (489 KB)
Request Information
Use our online request form
 
 
go to top of page | Print | Create PDF