Home Language Imprint Terms of Use www.bosch.com  1-800 REXROTH  
Bosch Rexroth
USA
Products and Solutions
Products
Industries
Trends and Topics
Documentation and Resources
Service
Training
How to Buy
Company
About Bosch Rexroth
Press
Company Overview
Press Releases
Rexroth Image Library
Trade Show Press Kits
2013 OTC Press Kit
2012 PACK EXPO Press Kit
2012 WORKBOAT Press Kit
2012 FABTEC Press Kit
2013 ATX West Press Kit
2013 WINDPOWER Press Kit
2012 MINEXPO Press Kit
2012 IMTS Press Kit
2012 AATExpo Press Kit
2012 ATX East
2012 OTC Press Kit
2012 NPE Press Kit
2012 ATX West Press Kit
2011 PACK EXPO Press Kit
2011 AATExpo Press Kit
2011 OTC Press Kit
2011 CONEXPO Press Kit
2011 ATX West
2010 PACK EXPO Press Kit
2010 ATE
2010 IMTS
2010 Semicon West
2010 ATX West
Archived: 2009
Archived: 2008
Archived: 2007
Archived: 2006
Archived: 2005
Archived: 2004
Archived: 2003
What's New
Trade Shows and Events
Jobs and Careers
Contact Us
  Contact Contact   Sitemap Sitemap  
image x  

[02.11.12]

Control block for winches

Winches are used for many applications on vessels both large and small, such as anchor hoisting, mooring of the vessel, and subsequent holding of the ship against the quay. Bosch Rexroth now introduces the HIWCB, a control block developed specifically for high-pressure hydraulic winches, specially intended for deck mounting, and with a modular design that enables interoperability with almost any type of winch.

The new control blocks for high-pressure hydraulic marine winches build on the developments underlying our existing control blocks. What sets them apart, is that they are entirely assembled from standard components. In other words: because they employ proven techniques and technologies, reliability is guaranteed. This is further underlined by the fact that these blocks come from a production line which is also used to manufacture products for the mobile industry. All components are carefully documented, and parameters such as tightening torques are measured, evaluated and documented. The incidence of component failure in the field is literally reduced to a minimum by this approach. And of course, standard components are cheaper than non-standard variants.

Modular design

What makes the HICWB unique is its modular design, which enables it to be combined with virtually any winch. This enables the vessel’s owner to hold fewer spare control blocks, and offers more options for dealing with changes. This is an improvement over control blocks designed specifically for a certain application or winch. Moreover, the new blocks can be combined with both axial and radial piston motors, and with their light weight of just 44 kg, they can even be directly motor-mounted.

In addition, each complete control block undergoes a specific treatment for maximum resistance to the extreme conditions offshore. The blocks themselves are galvanized and chrome-plated, and stainless steel is used for external moving parts such as the control lever and bushes. All adjustment elements have weatherproof covers. And as a final protective barrier, a triple coating is applied in layers of each 80 micron thickness.

Features

Besides the required standard functions like counter balance, relief and anti-cavitation valves, these lightweight and compact control blocks offer a range of additional features. To start with, they can proportionally control the winches or capstans used to raise or lower the anchor. The so called anchor break off function of the block, in combination with a variable displacement motor, enables the anchor to be broken free in a controlled manner. A three position hand lever valve is used for this function: in the break off mode, up to 1.5 times the maximum rated load is permitted. The second position of the valve allows the operator to select minimum speed (which can be pre-set) at maximum rated load, followed by maximum speed with minimum load at the third valve position.

A second important feature of the control block lies in the ability to maintain a constant tension on the mooring lines when the vessel is berthed. When the mooring lines slacken due to vertical movement of the vessel, e.g. during tide, wave motion or loading/unloading, the winches will wind in to maintain line tension. When the lines are tightened by vertical movement in the opposite direction, then of course the winches will pay out line. The system’s high responsiveness means that tension in the lines remains constant, avoiding overload and shock forces, and keeping the vessel firmly and securely moored against the quay.

Safety

Lastly, a number of safety features are integrated into the control blocks. An extreme situation can potentially occur when the hydraulic supply is cut off (for whatever reason) to a winch holding a suspended load, and without a brake applied. Oil can then leak via the motor drain circuit back to the tank, resulting in insufficient hydraulic pressure to continue holding the load. Ultimately, the motor will cavitate, and the load will drop uncontrollably.

To ensure a safe situation even in cases such as this, an extra valve is incorporated that responds to falling pressure by holding the oil in the motor, and blocking leakage to the tank. The motor will slow down, but will not cavitate, and the holding power remains assured.

Compact

Integrating the various features into the control block has made it possible to assemble a block that is highly compact. Not only does it require minimal space on deck, it also simplifies the integration of functionality in the installation, since it requires considerably less piping, and with fewer external couplings, the risk of leakage is even further reduced. This approach also drives down maintenance costs over the long term.

Finally, for all ship owners and builders there is the significant benefit of Bosch Rexroth’s global service network, offering the capacity and expertise needed to quickly and efficiently service or repair marine installations anywhere in the world.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros (6.8 billion) in revenue in 2010.

To learn more, please visit www.boschrexroth-us.com

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion ($71.5 billion) euros in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial.Additional information can be accessed at Further information is available online at www.bosch.com, www.bosch-press.com


(Magazine Note) Please Send Any Reader Inquiries To:

info@boschrexroth-us.com
Request Information
Use our online request form
Download Press Release (PDF 55 KB)
Download Image (JPG 49 KB)
 
 
go to top of page | Print | Create PDF