Press

Search press releases

2013-05-14
Photo-News

No overflow here!

The Dartford Creek Barrier is one of the most important elements in London’s flood protection system. Two gates, each weighing 160 tons, regulate the backflow of water into the River Thames and thus protect the towns of Dartford and Crayford from flooding.

 

2013-05-08
Statement

Quotes and statements at the bauma 2013

Stefan Spindler

“When it comes to investment decisions, total cost of ownership over a work machine's entire life cycle is playing an increasingly decisive role.”

 

2013-05-06
Product Information

Easy to integrate: Autarkic axes from Rexroth

With the drive concept “autarkic axis” Rexroth works on new machine concepts in close development partnerships with customers. Rexroth offers designers the advantages of hydraulic linear movements without the previously required investment into hydraulic power units and the associated pipework. The concept was realized in the form of a ready-to-install module with integrated, completely closed fluid circuit, a control block with digital valves and a hydraulic cylinder.

 

2013-04-30
Photo News

A pump for Brazil

A global product with local color. The high-efficiency, variable-displacement A10V axial piston pump has been enthusiastically received by the Brazilian market.

 

2013-04-30
Product Information

Multi-Ethernet axis controllers for hydraulic applications

IAC Ligna

In the woodworking industry dynamics and accuracy decisively determine the yield. For this reason, the precise control of tools is essential in order to produce in an efficient and cost-saving manner. With the new valves of the IAC series, Bosch Rexroth offers a very compact hydraulic drive system specifically for woodworking applications.

 

2013-04-29
Statement

Plastic Electronics: Flexible electronics open up new creative possibilities

Lucas Wintjes

"Plastic Electronics is a true source of innovative, visionary ideas. Applying electronic circuits onto thin, flexible materials, such as plastic film, is revolutionizing the product portfolio. The future will bring ultra-thin TVs, color screens for e-books, flexible RFID chips or foldable displays that can be rolled up like newspapers. However, translating these versatile product ideas from laboratory processes into series production requires new system concepts. Instead of batches and quantities, it is now about ongoing production."

 

2013-04-23
Photo News

International Noise Awareness Day: Quiet hydraulic pump protects residents and patients

Container compactors that compact waste start up several times a day – and that means noise. That noise can be especially disruptive in the vicinity of hospitals, care facilities, and in residential areas. To address this issue, Bosch Rexroth has developed a hydraulic pump for mobile container compactors that reduces noise by 15 dB(A) on average in relation to comparable pumps.

 

2013-04-10
Product Information

Bosch Rexroth sets new standards for excavators

VBO

Bosch Rexroth has put together high-performance components and a new software package that can significantly improve fuel efficiency of excavators. With the new DX340LC-3 (34 tons) and DX380LC-3 (38 tons) models – the latter being presented at bauma 2013 in Munich – the global manufacturer Doosan Infracore demonstrates how this technology works.