When a shredder at wood-based materials manufacturer Egger failed, Bosch Rexroth was quick to respond. In just four days, the fuel supply was not only back up and running but also future-proofed with modern Hägglunds drive units.
The town of Brilon in the eastern Sauerland region is not only the most densely forested town in Germany but also home to the largest site of the Egger Group, a leading international wood-based materials manufacturer with over 11,000 employees worldwide. The company produces around 10.4 million m³ of wood-based materials and sawn timber per year. The Brilon plant primarily produces chipboard and MDF boards for the furniture industry and specialist retailers.
A notable feature of the Egger plant in Brilon is its sustainable energy supply. Based on the belief that waste wood is too valuable to simply throw away, the wood is chopped into 40x40 mm pieces in two lines and transported to the company’s own biomass power plant to be used as fuel. The vapor is used to generate electricity via downstream turbines as well as to provide district heating for the sawmill’s drying chambers and other applications. “The plant’s electricity requirements exceed the annual consumption of the town of Brilon, which has around 25,000 inhabitants,” explains Nino Kapsalis, Head of Power Plant and Maintenance at Egger, to illustrate the output. “Thanks to the high efficiency of around 70 to 80%, our energy supply is virtually self-sufficient. However, at the beginning of 2025, it was briefly disrupted when one of the two fuel lines failed, and quick action was needed.”
The outage was caused by two pump failures that occurred in quick succession in the hydraulic power unit of the Pallmann Dracula single-shaft shredder, which shreds 300 metric tons of old wood per day for transport to the biomass chamber. After the first pump suffered damage without warning and had to be replaced, the second pump also failed just a few days later. “No other replacement pump was available, and delivery of the spare part from the US would have taken weeks,” recalls Michael Lenz, who heads up the Mechanics, Power Plant and MDF team at Egger. So, what to do? Nino Kapsalis’s team first reduced the boiler output and then procured a mobile wood chipper to increase the output again. However, the cost of renting this temporary solution was high. Over the total down time, the mobile chipper chopped approximately 2,200 tons of solid fuel.
In an effort to resolve the failure as quickly as possible, Lenz looked up the contact for Hägglunds at Bosch Rexroth. “That same day, we received a call from a very professional employee who discussed the situation with us and then a short time later presented us with three possible solutions,” recalls Lenz. “We had never experienced anything like this from our previous supplier.”
In view of the advanced age of the installation, Egger decided to replace the drive units. To bridge the gap, Bosch Rexroth supplied a rental unit from Hägglunds within three days, which was prepared in close consultation for plug-and-play connection to the existing control system. To enable direct integration, the unit was hydraulically modified in the Service Center in Bochum. Once on site, the experts at Egger made some adjustments to the electrical controls before installing and commissioning the unit together with the Hägglunds field service team. “Thanks to good preparation and coordination, we were able to continue using the existing peripherals to the greatest extent possible,” says Lenz. “Just five days after the second pump failure, everything was sorted and the fuel line was back to running normally.” “Thanks to the rapid action of Bosch Rexroth, we were able to return the mobile chipper after a short time, which significantly limited the rental fees,” adds Kapsalis.
The new Hägglunds DUc drive unit in the hall for supplying fuel (Image: Egger Gruppe).
The drive system of the single-shaft shredder (Image: Egger Group).
Egger is safeguarding the future operation of the two Pallmann shredders with two new Hägglunds DUc drive units. Like the previous solution, they feature a hydraulic direct drive that is connected directly to the shredder shaft without a driving gear, is resistant to impact loads and delivers the full torque even at low speeds. A further advantage of the direct drive is that any material jams can be eliminated immediately by reversing the direction of rotation. In addition, the application is more efficient, as the required flow rate of 260 l/min can be provided with a smaller sized unit.
Further important criteria for Egger were simple technology and high availability of spare parts. “The new drive unit is not only more compact, but also much simpler in terms of design, clearly structured and easier to maintain,” says Lenz. “For us this means maximum process reliability with planned maintenance and optimized spare parts inventory.” Egger also ensures a high degree of availability by means of a 5-year maintenance contract. For the duration of this period, the Hägglunds after-sales service will inspect the installation and provide recommendations for maintenance as required. In addition, the drive units are integrated into Egger’s monitoring system via sensors and control technology, which monitors over 20,000 operating parameters as a complete system for maintenance and process improvements. If needed, Egger also has access to the CytroConnect platform from Bosch Rexroth to implement supplementary data-based services, including predictive maintenance.
Kapsalis is certain that in Bosch Rexroth Egger has found a reliable and committed partner for the sustainable modernization of the hydraulics. A visit to the Hägglunds location in Bochum only serves to reinforce this assessment: “We are very impressed by the experience and capability of the Hägglunds team. We also really value the offer of internal training for fault finding on the machine, another part of the complete package offered.”
The project team from Egger and Bosch Rexroth (right to left): Nino Kapsalis, Valentin Loebert, Nelson Weber and Michael Lenz (Image: Egger Group).
As part of the next two overhauls of the biomass boilers, the remaining old drive unit is set to be replaced first, followed by the rental unit. “We assume that these projects will run just as smoothly as the first,” says Lenz. “The rental unit was delivered at 10 am, was put into operation by 7 pm and has been running smoothly ever since.” On the back of the positive experiences it has had so far, Egger has also commissioned Bosch Rexroth with a further modernization project: As part of the next two overhauls, the hydraulics of the push floors, which transport the fuel with a grain size of 40x40 mm from the day bunker to the combustion chamber, are also to be replaced. “We are extremely pleased with the rapid assistance, technical implementation and the overall concept of Bosch Rexroth,” sums up Kapsalis. “The decision to call Hägglunds was exactly the right one.”
Author: Valentin Loebert
Position: Account manager in the field
Sales Central Europe
Phone: +49 234 96639-199
Cell: +49 162 4347438
Valentin Loebert
Already connected on LinkedIn?
Valentin Loebert
Bosch Rexroth AG