Spain English
Assembly technology Accompanying picture hall
Assembly technology Accompanying picture hall

LogiMAT

  • Messe Stuttgart, Messepiazza 1, 70629 Stuttgart, Germany
  • 25/04/2023 09:00 - 27/04/2023 17:00
  • German, English
  • Electric Drives and Controls, Linear Motion Technology, Mobile Hydraulics and Electronics, Assembly Technology, Mobile Robotics

LogiMAT, the International Trade Show for Intralogistics Solutions and Process Management, sets new standards as the biggest annual intralogistics exhibition in Europe. This is the leading international trade fair that provides a comprehensive market overview and competent knowledge-transfer.

Get your tickets

NEXT LEVEL LOGISTICS

Are you looking to increase efficiency throughout your entire logistics chain and create complete transparency through intelligent solutions?

Then learn more about our customized solutions for your inbound, outbound and intra-logistics: get your logistics moving with Soft – and hardware components for forklifts and AMR as well as our extensive drive and control portfolio for high-stack storage and process automation. For demand-driven line supply, your stream of goods is singulated by AI-based Smart Item Picking via robot or Cartesian system according to the order and is transported fully autonomously to the point of need. Not even dynamic requirements will bring your flow of goods to a standstill, as we respond to any disruption or change in real time through our intelligently networked solutions.

Raise your logistics to a new level with compact hardware, flexible software, open interfaces and minimal engineering effort.

Contact us, we look forward to hearing from you.

We Move – You Win.

Visit us at our booth in hall 06 booth D31!


LogiMAT 23

Site map

Get your ticket

Enter your voucher and register

Your contact to Bosch Rexroth


The DAMBACH COMPACT SHUTTLE equipped with automation components from Bosch Rexroth in operation.

ctrlX AUTOMATION – automation toolkit for intralogistics

In intralogistics, many companies rely on automated logistics solutions to achieve greater efficiency. The open and flexible automation toolkit ctrlX AUTOMATION enables a reduction of the engineering effort by 30 to 50% and an efficient automation for example in combination with the robotics kit ROKIT. Another example of success is the COMPACT SHUTTLE from DAMBACH, which is controlled by the space-saving, powerful ctrlX CORE. The openness of the solution offers the possibility to add new functions to the shuttle at any time in order to remain future-proof and in motion.

Autonomous mobile robot ACTIVE Shuttle from Bosch Rexroth lifts up a dolly with 4 small load carriers.

The autonomous mobile robot (AMR) ACTIVE Shuttle is already making entry into the factory of the future!

The Factory of the Future is completely flexible and connected – AMRs fit perfectly into this type of environment, delivering goods to the point of need, exactly where and when they’re needed. There’s an increasing demand for multi-variant and small batch production, and ACTIVE Shuttle helps to solve this challenge, making intralogistics processes flexible but without having to change factory infrastructure. Future-proof and flexible in use, the ACTIVE Shuttle can also communicate with the fleet management software via the standardized VDA 5050 interface. This also makes mixed operation with mobile robotics from other manufacturers possible!
ACTIVE Shuttle

Kassow Robots five 7-axis cobot models: Payload up to 18kg, Reach up to 1800 mm, Speed up to 225 Degree/S.

Kassow Robots

Kassow Robots offers a wide range of five models to help all manufacturing companies, SMEs in particular produce even more competitively using cobots in a multitude of ways. True to the claim “strong, fast, simple”, the Copenhagen based company develops and produces uniquely efficient industrial collaborative lightweight robots with 7 axes. Despite their large reach up to 1800 mm, these cobots are extremely powerful, fast and suitable for use even in confined spaces – Kassow Robots cobots are able to reach around corners. These innovative robots enable SMEs to achieve complex automation and programming flexibly, independently and cost-effectively.

Rexroth ROKIT key visual consisting of four overlays for the respective product names.The lettering UX is shown in the center. It is surrounded by a circle with a red border, which consistsof buttons named software, hardware and service. Respective product icons are placed next to them. Below the icon, five mobile robots are lined up.

Level up your mobile robots – with the robotics kit ROKIT

The modular robotics kit ROKIT of proven software and hardware components unlocks new possibilities for market players. It offers maximum flexibility, and efficiency in the automation of processes. The components – ROKIT Locator, ROKIT Navigator, and ROKIT Motor – take care of positioning, navigation and motion execution and come with the intuitive graphical user interface aXessor.
Together with crtlX AUTOMATION, we will present an example of how you can use our open automation toolbox of software and hardware components to tailor and automate your mobile robots to your needs.

Robot arm surrounded by boxes filled with objects. The arm grabs an object that says "Factory of the future".

Software for autonomous handling of unknown objects with industrial robots

Using Smart Item Picking as an example, we will show you a software solution that enables the autonomous handling of objects by commercially available industrial robots. In this application, it automates manual picking tasks and processes in logistics, such as in goods distribution centers. The software recognizes a large number of objects to be gripped model-free without teaching and with the help of artificial intelligence. The solution can be adapted to individual customer requirements and does not require a specialist to operate. High pick rates increase productivity, compensate for capacity bottlenecks, and significantly reduce error rates.

Linear technology solutions for your application in the logistics industry

Linear Motion Technology – intelligent options for sustainable logistics solutions

From individual components to smart mechatronic subsystems – Rexroth linear technology offers fast, efficient and future-oriented solutions for the logistics industry.
Increase productivity, promote sustainability at the same time and save resources: The electromechanical cylinders guarantee a long service life and are not only economical but also energy-efficient and low-maintenance.
Ready-to-install linear axes, for example with toothed belt drive, are compact and light, but at the same time have a high rigidity. They are perfectly suitable for use in packaging, logistics and storage lines.
Plug and Produce with our new linear robots – consisting of best-in-class linear technology components, automation hardware and software. The ideal solution for your automation requirements.

BODAS – Intelligente Elektronik & Telematik für Mobilanwendungen

BODAS Mobile electronics & Telematics

With BODAS - Bosch Rexroth Digital Application Solutions - we offer a holistic ecosystem from IoT telematics to software and electronic hardware, like sensors displays and control units, for the off-highway market.
BODAS is open, scalable and provides easy access to put less strain on your resources and increase your profitability. It combines expertise as well as application know-how and is defined by market-leading quality and future-proof solutions. This applies to standard products but also to jointly developed customized solutions.

Multi-camera system for industrial trucks and off-road vehicles

Multi-Camera System

The Bosch sight assist monitors the areas in front of, behind and to the sides of the forklift, providing a 360-degree surround view. By glancing at the display, the driver can see exactly how much space is left to maneuver. In addition, the driving lane of the forklift can be shown in the display image depending on the steering angle. The Bosch sight assist comes with a user-friendly application concept that makes it possible for you to adapt the system to different vehicle variants with a software tool. In order to meet the demand for equipping existing machines, Bosch will also offer the multi-camera system as a retrofit solution starting in 2023.

Automated vehicle maneuvering – plant optimizes the production workflows in the automotive industry

Automated valet parking – the world’s first driverless parking service

Bosch has developed automated valet parking, the world’s first highly automated driverless (SAE Level 4) parking function to be given official approval for commercial use in Germany. All the driver needs to do is stop the vehicle in the designated drop-off area and get out. The smart Bosch infrastructure installed in the parking garage then takes over and interacts with the technology in the vehicle to drive it to the vacant space and park it. APCOA’s P6 parking garage at Stuttgart Airport is the first in the world to enable commercial use of the driverless parking system.
The principle of automated valet parking also offers advantages in other areas – for instance in the automotive industry: Automated vehicle maneuvering - plant significantly optimizes the production workflows. The system maneuvers new vehicles driverless from end of line, e.g., to loading stations and also to the customer center.