Image of illustrated interlocking hands and of the resistance welding control PRC7000 from Bosch Rexroth Welding spot on – for unbreakable connections

Rethinking welding technology. With the PRC7000 welding control, you can master any challenge

Resistance Welding –
Not all types of welding are the same

Difficult material combinations, higher expectations in terms of quality and productivity, and new system technologies require greater performance in welding. At the same time, Industry 4.0 capability is in demand in modern factories. Bosch Rexroth has the answer with the welding control PRC7000. It enables precision welding of different materials and has functionalities to make processes future-proof and simpler.

Discover, what makes us the leading Resistance Welding provider:

Our welding systems make you fit for the future

Bosch Rexroth is an innovation driver and role model in the global welding industry – and has been for over 60 years. In addition to our outstanding engineering skills, our pioneering role also constantly challenges us to make our technologies compatible with the requirements of the Factory of the Future. With integrated IoT interfaces, AI-enabled hardware components and web-based control solutions, we are setting the course for a seamless transition into the future.

We offer you a comprehensive solution

What makes an excellent resistance spot welding range? It is wide-ranging and offers versatile software and hardware solutions from a single source – or just the exact components that are needed. This is also reflected in our own range: It is freely scalable and thus enables both customized and pragmatic system solutions. Our many years of experience, which we have gained in cooperation with various industries, make us a unique supplier of welding technology on the market and coherently round off our range of products.

Our strength, your gain: adaptability

Adaptability is the core competence when it comes to evolving with the ever-changing demands of the industry and individual sectors such as the automotive industry. The joy of change and transformability is not only reflected in our attitude, but also in the characteristics of the technologies and processes; be it adaptive controls, real-time quality monitoring or web-based engineering tools – to name just a few aspects.

Take your welding systems to the next level

Master every challenge with confidence with the future-oriented and scalable solution portfolio for resistance spot welding from Bosch Rexroth. Our welding controls and medium frequency welding transformers make a decisive difference for you – in terms of performance and efficiency:

Expand your capabilities with direct control of the 7th axis. Our control system captures and interprets the additional process signals from this servo axis to intelligently regulate the welding cycle/operation and take quality to a new level. At the same time, you can significantly optimize other processes, such as end milling. Choose a fully integrated solution for greater efficiency and precision throughout your entire welding system.

Illustrated lightbulb.

Intuitive operation. Reduced costs.

Increased complexity and requirements in resistance welding meet a shortage of skilled workers. The welding control system PRC7000 makes welding simple – even for untrained users. The Functional Bundle "Simplicity" provides components such as PRIweb" and "Auto Reference Curve Creation".

The web-based user interface "PRIweb" stands for simple and intuitive usability. It thus offers advantages over the classic PRI7000, especially for unskilled users. The function is designed for use on mobile devices such as tablets. Users are provided with an intuitive user interface that allows them to quickly find and operate special functions, for example.

The "Auto Reference Curve Creation" function addresses two important capabilities of the welding control PRC7000: adaptive control and monitoring. For these, control curves must initially be recorded and activated. Until now, this required a high level of domain knowledge. This process can now be automated, which reduces the effort and ideally improves the result.

Illustrated stopwatch.

Less spatter. Highest productivity.

Resistance welding in record time. The "Dynamic Squeeze Time" and "Adaptive Spatter Reduction" software components, which are part of the "Productivity" license package, simplify resistance welding – for example in automotive production. The result: higher productivity, quality optimization and reduced workload for users.

"Dynamic Squeeze Time" reduces the hold-off time depending on force and position. The feature can only be used in conjunction with the integrated gun control. Overall, this results in reduced hold-off time and increased productivity by shortening the production process.

"Adaptive Spatter Reduction" also focuses on savings and supports weld parameter optimization during the commissioning phase and series production of the car. Welding parameters are automatically optimized in terms of quality and spatter rate as well as energy efficiency and limit values. For example, weld spatter occurring during the welding process can be automatically detected and minimized within a predefined tolerance band.

Illustrated human brain.

Artificial Intelligence. Real future opportunities.

The welding control system of the future is intelligent and draws benefits from the data generated in the welding process. This data can form the basis for process optimization and value creation in Industry 4.0 – for example, through self-learning processes and predictive maintenance. To do this, they must be collected, analyzed and processed. With the "IoT Connector" from Bosch Rexroth, users can easily collect data treasures, process them according to their needs, and implement automatic logging for quality assurance, for example.

Illustrated open-end wrench and screwdriver.

More service. Less downtime.

Where does good service start and where does it end? Ideally, it accompanies the entire life of a welding control system – and beyond. The Bosch Rexroth service portfolio for resistance welding ranges from commissioning through to the second life of a product. In addition to various services for optimizing the welding process, the services for the entire life cycle also enable a longer product life of the welding control system as well as resource conservation. For example, used control units are given a new lease of life through remanufacturing.

With its welding services, Bosch Rexroth is breaking new ground in the industry. Until now, the focus in welding technology has often been on the hardware. But it is the services that make welding control systems fit for the challenges of today and tomorrow.

PRI7000 – user interface for the welding controller PRC7000

GUI

PRI7000 for programming, operation and diagnostics of the PRC7000.

Medium-frequency system PRC7000

Controls

Medium frequency system PRC7000 for spot and projection welding applications.

System components of the welding controller PRC7000

System components

To extend the functional possibilities of the welding control.

Medium Frequency Welding Transformers

Medium frequency welding transformers

Optimized for more power and efficiency in resistance welding.

Resistance Welding - Blog Overview

News & Trends

In our blog you will find insights and valuable information about Resistance Welding Solutions from Bosch Rexroth.

Latest Blog Articles

Support

Service for process control

Service for Resistance Welding

Our services
Contact Bosch Rexroth

Contact us!

Contact Locator
Training for Process Control

Training

Bosch Rexroth Academy

In the Bosch Rexroth Academy we offer tailor-made training and qualification for technical experts.

Our training is practice-oriented, tailored to the respective target group and is based on the latest teaching methods and trends.

Find your training
Find your training

Training overview

Training program

Training program

The current training program of the Bosch Rexroth Academy for download.

Contact

Contact

Find out everything about training.

Video

Video

Watch the Industry 4.0 training video.

Quick access to process control material

Get in Contact with us!

E-mail:
sales.resistance-welding@boschrexroth.de

Information sources