United Kingdom

Select your location

United Kingdom
 

Press

Content
DC/787 2017-05-24

Bosch Rexroth factory achieves substantial cost savings with integrated measuring systems

Leading drive and control specialist Bosch Rexroth has reported two years of maintenance-free production at its plant in Schweinfurt, Germany, following the installation of its own Integrated Measuring Systems (IMS), a move that has saved the company tens of thousands of Euros in maintenance and running costs.

The plant, which manufactures high-precision linear motion components such as profiled rails, runner blocks and ball screw drives, as well as entire linear motion systems, has not experienced a single instance of machine downtime, while producing materials with a repeatability of +/- 0.25 µm.

Bosch Rexroth has now converted its cost savings into a “Total Cost of Ownership“ tool, which allows manufacturers to calculate their own savings, as well as the potential savings for mechanical engineers and end users.

Linear motion systems require a high level of accuracy in order to function properly. For example, the highest accuracy class, UP, has a height and parallelism tolerance for profiled rails over 1000m of just 3µm. By meeting minimum tolerances, manufacturers can ensure their products are interchangeable with others of the same size.

Until 2014, Bosch Rexroth relied on optical position sensors, or glass scales, to achieve the desired accuracy with its metal-cutting equipment. These solutions were expensive because they required regular cleaning and maintenance. At times, they were even responsible for machine failures because they were prone to introducing contaminants.

Optical position sensors can cause substantial downtime because they have to be physically removed in order to be cleaned thoroughly, before being reinstalled, realigned and recalibrated. They also halt production once a year because the measuring signal of each optical system must be tested, costing more hours in downtime.

Bosch Rexroth installed integrated measuring systems (IMS) into its ball and roller runner blocks. The IMS, which can detect the absolute position of an axis down to +/- 3 µm/m, are integrated completely into each machine, saving on installation space. They are resistant to vibration, shock and magnetic interference, and do not wear over time because they measure using induction.

Unlike optical sensors, they also function without sealing air systems, saving time and costs in the maintenance of oil separators and particle filters, and reducing the risk of contamination to the machine.

Any downtime is significantly reduced because each component can be replaced individually, with any repairs taking less than an hour. The measuring systems also integrate seamlessly into a wide range of automation systems, including DRIVE-CliQ , HIPERFACE , and SSI and TTL interfaces.

Stefan Dorn, Head of Advanced Engineering and Technical Product Management for Linear Motion Technology at Bosch Rexroth, said:

“Accuracy requirements are becoming more exacting in virtually every metal machining sector and application. This also increases the degree of accuracy required for linear motion technology and measuring systems. To meet this challenge, Bosch Rexroth has been using its maintenance-free IMS solutions in upgraded machine tools for more than two years.

“Since replacing the glass scales, we have achieved five-figure savings in terms of maintenance costs and availability. IMS also have the potential to decrease system and assembly costs for machine manufacturers.”

To find out more about Bosch Rexroth’s range of Integrated Measuring Systems please click here

 

Search press releases


Contact

Lynsey Cutler
15 Cromwell Road, St Neots 
PE19 2ES Cambridge
Phone: 01480 223290
Lynsey.Cutler@boschrexroth.co.uk

Related Articles

2014-06-24
Product Information

Industry warned of grey repair threat to hydraulic and electronic drives

Non-official or ‘grey’ repairs to hydraulic and electronic drives are threatening industrial productivity by increasing downtime and placing warranties at risk, according to one of the UK’s leading drives and controls manufacturers.


2014-06-24
Ergonomics

Manufacturers must do more to tackle poor ergonomic design

More than 7.5 million working days lost every year as a result of musculoskeletal disorders (MSD)