United Kingdom

Select your location

United Kingdom
 

Press

Content
DC645 2012-11-21

Innovative Rexroth Range Is Celebrated For Its Energy Efficiency

Innovative Rexroth Range Is Celebrated For Its Energy Efficiency

Rexroth’s innovative variable speed pump range Sytronix, has been shortlisted in the Energy Awards 2011 as a leading energy and cost effective solution.

One of the variable speed pump models in the Sytronix range Rexroth’s innovative Sytronix variable speed pumps have been recognised by the Energy Awards 2011 in its Energy Efficient Product of the Year category.

The Sytronix range provides the best of both worlds – the reliability of powerful hydraulics with the energy efficiency and dynamics of compact eletronics and variable speeds. Plus, energy savings of between 30% and 80% provide a rapid return on investment.

Andrew Collins, Machinery Applications and Engineering Sales manager at Bosch Rexroth, said:” In pressure generation, the use of innovative Sytronix speed-variable pump drives offers great potential for saving energy costs and reducing noise pollution. These results are achieved by reducing the speed of the electric motor and thus the power consumption thanks to intelligent frequency converters.

“Having the Sytronix range shortlisted in the Energy Awards 2011 is a great privilege and we’re excited to hear the result in December.”

Rexroth Sytronix comprises of a comprehensive modular system of pumps, controllers and motors as well as software. Depending on the cycle characteristics and configuration, the variable-speed pump drives can reduce energy consumption in the most varied applications by 30 to 80 percent.Further information on Bosch Rexroth can be found at www.boschrexroth.co.uk.

 

Search press releases


Contact

Melanie  Bright
15 Cromwell Road  
PE19 2ES Cambridgeshire
Phone: 01480 223 290
press@boschrexroth.co.uk




Related Articles

2016-11-30
Press Release

Silence is golden: New development in low-noise gear pumps for mobile applications

Diesel exhaust and noise pollution is an increasing concern for businesses, but for the agricultural sector it has always been an issue. Hydraulic systems have many applications and benefits, but few people would associate their use with a quiet working environment, until now.


2015-11-26
Press Release

The requirements of conveyor systems are more demanding than ever. We provide a versatile, high performance conveyor system wiith our modular, standardised solution which can be used across multiple i

Contaminated oil has been identified as one of the key causes of hydraulic system failures, which can lead to machine failure and critical production downtime.