United Kingdom

Select your location

United Kingdom
 

Press

Content
DC639 2013-05-30

Safety Given Top Priority at Europe’s Largest Dam

Safety Given Top Priority at Europe’s Largest Dam

The Deriner Dam is one of Europe’s largest – and thanks to hydraulics from Rexroth, it is also one of the safest.

The dimensions of the Deriner Dam on the Coruh River in north-eastern Turkey are gigantic in every respect. Over 3.5 million cubic metres of concrete were poured into this 249 metre high and 720 metres long structure. Construction has been going on for ten years, with a budget that has grown to €1.5 billion.

The heart of this mammoth project is an underground hydroelectric power plant. Every year, four giant turbines will generate 2,100 gigawatt hours – the annual consumption of a big city.

“To achieve this power output, we will impound almost two billion litres of water,” explains Hilmi Kaplan, who is responsible for the electromechanical realisation at ERG Trade and Industry. Since the 1970s, this Turkish company has specialised in major infrastructure projects and is responsible for large portions of the dam construction. “Safety is naturally a top priority in any project of this size,” continues Kaplan. “The main risk for a dam is that the reservoir overflows, which would result in uncontrolled flooding. This could potentially be caused by earthquakes or extreme tides in the nearby Black Sea.”

Priority for safety

Two large tilting gates, which feature Rexroth drives, provide flood discharge capability. The gates divert surplus water into the basin at the foot of the dam via two artificial diversion tunnels.

“A total of 2,250 cubic metres per second can run off via these ducts,” Kaplan summarises. “That’s enough for a lot of situations. But if a ‘flood of the century’ should occur, we need many times this capacity.” For this reason, eight central outlet gates have been integrated into the main dam structure. These gates can handle an additional volume of around 7,000 cubic metres per second. The openings are arranged symmetrically in order that all eight water flows intersect just above the surface of the downstream basin. This reduces the impact of the outflowing water.

As a project partner of ERG Trade and Industry, Bosch Rexroth was responsible for the drive and control solution for the central outlet gates and the two tilting gates. The local branch office supported the conceptualisation, assembly and installation, together with specialists in Germany. “The great advantage for us was that we had just one partner for all flood discharge issues. In effect, we were supplied a turnkey system,” explains Kaplan.

The opening drives for the massive central outlet gates represented a major challenge for the design of the hydraulic drives. Each gate is 2.8 by 5.6 metres and weighs 24 tonnes. Despite this weight, the corresponding drives must work in parallel with a high degree of precision to ensure that the gates always open and close in sync. This causes the streams of water to meet above the basin, thus dissipating their energy. This is essential to prevent erosion of the valley walls and the undercutting of the dam.

The solution was to mount the drive cylinders of the central outlet gates vertically in the drives. In addition, the cylinders are made of lightweight special steel. “We were also subject to extreme constraints in the weight of the cylinder,” adds Kaplan. “Each component of the dam could only be lowered using a special cable crane with a load capacity of 30 tonnes.”

Delay-free synchronisation of all the gates is essential for efficiently opening and closing these additional flood discharge mechanisms as needed – but the sensor signals need to cover distances of up to 1,250 metres. “For this reason, a fibre optic network is used in the dam to transport each control command.” Like the central outlet gates, this network has also been installed and fully tested, so that the Deriner Dam can safely go into service in 2013.

 

Search press releases


Contact

Melanie  Bright
15 Cromwell Road  
PE19 2ES Cambridgeshire
Phone: 01480 223 290
press@boschrexroth.co.uk



Related Articles

2014-09-05
Press release

Wave industry leaders and Bosch Rexroth join forces to develop a standardised offshore power system

A number of leading wave energy firms have joined forces with global drive and control manufacturer Bosch Rexroth in a bid to create a standardised, self-contained offshore electricity generator for the wave industry.


2014-06-24
Product Information

Industry warned of grey repair threat to hydraulic and electronic drives

Non-official or ‘grey’ repairs to hydraulic and electronic drives are threatening industrial productivity by increasing downtime and placing warranties at risk, according to one of the UK’s leading drives and controls manufacturers.