United Kingdom

Select your location

United Kingdom
 

Press

Content
DC636 2013-06-19

Bosch Rexroth Gives Some Legs to Walking Robot

Bosch Rexroth Gives Some Legs to Walking Robot

The “Mantis” hexapod robot is aimed at applications both in the film industry and other sectors, such as unmanned subsea exploration, and work in environments that are sensitive to terrain damage.

Mantis, the world’s biggest operational all terrain hexapod robot, which was unveiled earlier this year, has made an appearance at the Elmia Wood 2013 forestry exhibition (5 – 8 June 2013) in Sweden. The nine foot (2.7 meters) tall robot, which resembles a giant insect and can be driven remotely or piloted from the machine’s cockpit, took four years to develop and features Bosch Rexroth components and know-how.

18 Rexroth 4WREE6 valves provide the integral function of controlling the hydraulic cylinders that operate the Mantis’ six legs. Each leg features three independent closed loop axes, one at the knee and two at the hip, with feedback provided by sensors installed on the outside of the leg.

Mantis is the brainchild of chief designer Matt Denton, managing director of Micromagic Systems, who first decided upon the concept and created the computer controls that give the machine its high functionality. These include the ability to move omnidirectionally (forwards/backwards, crab left/right, turn left/right), climb over uneven ground and raise and lower on command.

Speaking about the machine’s development Matt said: “I’d been making smaller hexapod robots for a number of years for use in the film and TV industries as well as for private collectors. I felt that if I could scale up the machine to the point where it could carry a person that, as well as demonstrating what is possible with current technologies and British engineering, there could be further applications both in the film industry and other sectors, such as unmanned subsea exploration, and work in environments that are sensitive to terrain damage.

“I was aware of Bosch Rexroth valves from their use in special effects on films I’d worked on in the past. Having contacted Bosch Rexroth I was put in touch with Nigel Hart who, as well as specifying the Rexroth 4WREE6 valves, provided assistance and advice on the hydraulic design of circuits, safety considerations, reducing the reservoir size and cooling. What impressed me most about the Bosch Rexroth valves, and proved essential to the functionality of the machine, was the smooth and accurate control they provide.”

In addition to the 18 Rexroth 4WREE6 valves Mantis features a Rexroth A10VO63DFR pump, typically used in booms and cranes that supplies the robot’s hydraulic power. Fitted with load sensing the pump ensures that only the right flow and pressure is delivered reducing power consumption.

Nigel Hart, sector manager for Marine and Offshore at Bosch Rexroth UK said: “Mantis is a fantastic demonstration of what can be achieved with today’s technology. It is also indicative of the significant changes that have happened throughout the industry over the past ten to fifteen years. Now even the most simple of components come with intelligence that allows it to perform a variety of functions and adapt to a number of applications.”

 

Search press releases


Contact

Melanie  Bright
15 Cromwell Road  
PE19 2ES Cambridgeshire
Phone: 01480 223 290
press@boschrexroth.co.uk

Related Articles

2016-11-30
Press Release

Silence is golden: New development in low-noise gear pumps for mobile applications

Diesel exhaust and noise pollution is an increasing concern for businesses, but for the agricultural sector it has always been an issue. Hydraulic systems have many applications and benefits, but few people would associate their use with a quiet working environment, until now.


2015-11-26
Press Release

The requirements of conveyor systems are more demanding than ever. We provide a versatile, high performance conveyor system wiith our modular, standardised solution which can be used across multiple i

Contaminated oil has been identified as one of the key causes of hydraulic system failures, which can lead to machine failure and critical production downtime.