United Kingdom

Select your location

United Kingdom
  • Home
 

Press

Content
DC630 2013-03-28

Bosch Rexroth Launches Innovative Range of Press Blocks

Bosch Rexroth Launches Innovative Range of Press Blocks

Bosch Rexroth has extended its range of hydraulic press blocks with a new series specifically aimed at machine builders supplying press machines to a wide range of metal and other plastic / composite forming applications.

The type M modular press blocks will make it significantly easier for machine builders to achieve EN 693, EN 289 and ISO13849. The press blocks are ideal for upper rams on downstroking presses and have been specifically designed for both new build presses and retrofit on existing machinery.

The new range includes a new safety feature, namely hydraulic circuit configuration with monitored directional control valves. Flexibility has also been prioritised with a primary module providing free fall with proportional valve tonnage control. Additional modules can be fitted for extra press cylinders which will allow other functions such as regenerative flow, high and low pressure control and load sensing.

The Rexroth type M modular press blocks offer a flow rate of up to 1300lpm and system pressure of up to 350 bar. The range compliments the existing Rexroth range (types P, B, L and S) which can handle flow rates up to 14000lpm.

Alan Simpson, specialist sales manager for presses and production machinery at Bosch Rexroth, commented: “The type M modular press blocks have been designed with flexibility in mind, making them suitable for a wide range of presses in numerous industry sectors. The new press blocks meet the critical industry standards and regulations which will make press block specification much easier for machine builders.”

 

Search press releases


Contact

Melanie  Bright
15 Cromwell Road  
PE19 2ES Cambridgeshire
Phone: 01480 223 290
press@boschrexroth.co.uk




Related Articles

2016-11-30
Press Release

Silence is golden: New development in low-noise gear pumps for mobile applications

Diesel exhaust and noise pollution is an increasing concern for businesses, but for the agricultural sector it has always been an issue. Hydraulic systems have many applications and benefits, but few people would associate their use with a quiet working environment, until now.


2015-11-26
Press Release

The requirements of conveyor systems are more demanding than ever. We provide a versatile, high performance conveyor system wiith our modular, standardised solution which can be used across multiple i

Contaminated oil has been identified as one of the key causes of hydraulic system failures, which can lead to machine failure and critical production downtime.