United Kingdom

Select your location

United Kingdom
 

Press

Content
DC624 2012-11-02

New Rexroth Pump Can Save 10,000 Litres Of Diesel

New Rexroth Pump Can Save 10,000 Litres Of Diesel

Specifically tailored to market needs: The A1VO variable displacement pump from Rexroth enables the economical use of energy-saving load-sensing systems even in smaller tractors.

The A1VO axial piston variable displacement pump designed by Rexroth especially for the segment of small tractors reduces diesel fuel consumption by around 10,000 liters over the entire useful life of 6,000 operating hours. The new variable displacement pump reduces the cost differential compared with constant displacement pumps so greatly that it enables for the first time an economical switch from the traditional open-center design to a load-sensing system. This approach summons hydraulic power as it is needed. Simulations based on a 90 hp diesel engine actually used in the marketplace verify fuel savings of between ten and 15 percent per operating hour in mixed usage.

In larger tractors load-sensing systems as a consumption- and thereby emissions-reducing technology have already proven themselves. But for the very price-sensitive segment of small tractors this technology has until now been unaffordable. Rexroth has therefore tailored the design of the new A1VO variable displacement pump to the needs of this market segment – for example by relocating all the connections to the port plate and significantly reducing the number of different models. This simplifies manufacturing, which helps the small-tractor segment achieve a commensurate price/performance ratio.

To make the switch easier for tractor manufacturers, the A1VO has similar dimensions and performance data to the otherwise generally used constant displacement pumps. With a suction volume of 35 cm3 it is designed for speeds up to 3,000 rpm. The variable displacement pump achieves a working pressure of 250 bar and a peak pressure of up to 315 bar and moves up to 105 l/min. The efficiency is nearly 90 percent. Service life is comparable to the A10VO and A10VNO version used on the large tractors.

In comprehensive simulations using OEM engine map data of a commercially available 90-hp-diesel Rexroth calculated consumption savings of between ten and 15.9 percent per operating hour. The results also took into account varying load cycles: from pure travel mode with zero hydraulic output to partial-load operation and full-load operation of the working hydraulics.

The new pump achieved the greatest savings in diesel fuel consumption in partial load operation such as holding the plow during transport or working with the front loader. Projected on to the usual life expectancy of 6,000 hours and assuming a typical load cycle distribution, an overall savings of around 10,000 liters of diesel fuel can be expected.

 

Search press releases


Contact

Melanie  Bright
15 Cromwell Road  
PE19 2ES Cambridgeshire
Phone: 01480 223 290
press@boschrexroth.co.uk




Related Articles

2014-06-24
Product Information

Industry warned of grey repair threat to hydraulic and electronic drives

Non-official or ‘grey’ repairs to hydraulic and electronic drives are threatening industrial productivity by increasing downtime and placing warranties at risk, according to one of the UK’s leading drives and controls manufacturers.


2016-11-30
Press Release

Silence is golden: New development in low-noise gear pumps for mobile applications

Diesel exhaust and noise pollution is an increasing concern for businesses, but for the agricultural sector it has always been an issue. Hydraulic systems have many applications and benefits, but few people would associate their use with a quiet working environment, until now.