Press

Content
DC616 2011-07-11

Tip top condition

Tip top condition

HMU

The wind power industry faces enormous challenges in monitoring the condition of wind turbine blades. Stuart Williams, Renewable Energies Control Products Manager at Bosch Rexroth, analyses the problem and offers an innovative solution.

Wind power has been identified by the Government as one of the key technology platforms to enable the UK to achieve its carbon emissions and climate change targets. However, whilst wind power is environmentally friendly, it is not without issues of its own, most notably how to ensure that turbines remain operational for long periods in often harsh climatic conditions. In particular, rotor blades are among the most accident sensitive components of a wind turbine and if damaged, one of the most expensive parts to replace. The condition monitoring of rotor blades is normally carried out on a periodic basis with long intervals between inspections. This can be problematic, as a small easily rectifiable fault can grow to something much more serious.

What’s more, the planned growth in offshore installations means that maintenance will be more problematic. For example, the North Sea only has a three-month service and maintenance window each year.

The most common problems with wind turbine blades are excessive load, lightning damage and ice formation.Ice protection is particularly important to protect people, animals and property around the wind turbine from ice shedding as the blades turn. Monitoring systems have to be able to react very quickly to swiftly shut down the rotor blades if required. If blades that are ice covered are not stopped there is potential for ice to be hurled around. Secondly, blades covered in ice can cause structural damage due to overloading, including blade cracking.

The traditional method of monitoring blades is to either use dual anemometers (one heated) or to monitor the ambient conditions to try and predict when ice will form. Neither method is accurate and will not monitor the build-up of ice on the blades. If ice is suspected, the wind turbine is normally shut down and a physical inspection is undertaken when it is believed the ice may have cleared. This is not an exact science and can lead to an excessive amount of generation being lost during winter spells.

A second key issue is cost-related, namely that early detection of small defects, like trailing edge cracks or delaminations, can be repaired easily with a simple one-day trip by an engineer. However, if left undetected, these cracks can cause major structural damage which take much longer to repair and can become more costly. However, getting engineers to travel to often remotely located wind turbines can be costly. The answer may lie in using the natural oscillation of the turbine blade to determine the blade’s true condition. Rexroth’s BLADEcontrol is a system that continuously monitors the condition of the rotor blades on wind turbines and immediately signals to the operator and/or the machine control of problems such as structural blade damage, ice build-up or lightning damage. What’s more it can keep track of the history of the blades condition to offer an on-going forensic trail of wind turbine performance.

BLADEcontrol performs an analysis of the natural oscillation frequencies of the turbine blade which change when the blade is damaged or has a greater dynamic load, such as when ice forms. The frequencies of a rotor blade can vary within a typical range of up to around 350 Hertz. This distribution of frequencies is essentially the fingerprint of the blade. Distinctive frequencies arise when ice is formed due to the ice on the rotor blade being heavier causing a slower oscillation. These specific frequency peaks are easily visible on a monitor. Structural damage is visible within the low frequency range, whilst minor damage is only visible within the higher frequency range. For example, slight rotor blade damage, such as multiple trailing edge cracks will not affect the spectrum between 0 Hz and 50 Hz but visible changes are noticeable between 150 Hz and 250 Hz.

The Bosch Rexroth system works via the attachment of accelerometer sensors (multi-dimensional piezo-electric accelerator sensors), which are glued directly into the rotor blades. A data collector in the hub converts the analog, measured oscillations into digital values and transmits these from the hub into the nacelle via WLAN. The digital data is then interpreted by the BLADEcontrol embedded processing unit.

The data is recorded online and evaluated in detail in the BLADEcontrol embedded processing unit in real time. If, at any point, an extreme event occurs, such as serious damage to the blades or ice on the rotor blade, the control system is immediately informed that the system is to be stopped. A further benefit is that as the blades are being monitored locally even when stopped as there is still wind blowing over them, the Rexroth BLADEcontrol system can perform an auto restart when all ice has cleared. This obviously removes the need for an engineer to visit the turbine and also keeps lost power generation to a minimum

In terms of maintenance work, BLADEcontrol can differentiate between small, non-threatening edge cracks and major structural damage. This allows for the introduction of a planned maintenance schedule rather than a reactive schedule.

Calculations suggest that a control system such as BLADEcontrol could generate a payback period of less than two years by early detection of repairs, lower insurance costs, savings on maintenance costs and reduction in unnecessary downtime leading to higher yields. For many wind farm operators there is also the added benefit of peace of mind that their expensive asset is in top condition and fully operational.

Case Study Box Out

Andreas Reichl operates the Sternwald Windpark, Upper Austria’s largest windfarm, which is equipped with a single Vestas V80-2 MW and six V90-2MW, with 100 metre high hubs.

The seven towers in Sternwald stand at a height of around 1,000 metres, where it is often very windy. Also, in winter there’s also considerable ice and snow. The build-up of hoar frost in particular, poses a challenge for wind farm operators causing ice on the rotor blades. “We weren’t happy with the built-in system that we had used up to that point, as it was displaying completely false readings. What’s more, the previous system frequently switched off much too late, but did not allow the turbine to operate when free of ice.”

Reichl turned to Rexroth’s BLADEcontrol. “A measurement on the nacelle will always be inaccurate. If you want to know whether there’s ice on the blades, that’s where you have to measure it,” says Reichl who has also benefited from being able to implement a preventive maintenance programme. “One day our system displayed an unexpected change in the spectrum. It transpired that the dampers of a hydraulic adjusting element (pitch control) were defective. Bosch Rexroth’s system had registered this interruption without knowing the reason. Major damage was avoided.”

 

Search press releases


Contact

Stuart  Williams
15 Cromwell Road, St. Neots 15
PE192ES 
Phone: +44 (0) 1480 223200
Fax: +44 (0) 1480 470 789
stuart.williams@boschrexroth.co.uk




Related Articles

2013-03-05
Product Information

Keeping the blades turning - Ice Detection

As rated power for wind turbines increase, the cost of blades increases dramatically. John Reimers, an expert in wind turbine blade monitoring systems at Bosch Rexroth, examines the issues and offers a potential solution.


2012-11-02
Product Information

Rexroth lifts wind energy to new heights

With its first successful delivery of an advanced hydraulic jacking system coming five years ago, Rexroth has announced a further three wind turbine installation vessel projects.