United Kingdom

Select your location

United Kingdom
 

Press

Content
DC701 United Kingdom, 2014-09-08

Bosch Rexroth Encourages Smart Agriculture through Innovative Components

The Automatic Hitch Control (AHC) dynamically regulates the relationship between position and tractive force, independent of the implement. This enables optimum soil tilling performance, increasing yields and hence saving fuel.

With these new developments, Bosch Rexroth is supporting the most important aims of today’s agricultural technology - sustainably securing yield capability, increasing efficiency, and conserving resources.

The operator simply needs to select the optimum tilling depth. The dynamic of the AHC is based on adaptive control algorithms and sensors that continually measure the hitch height and tractive force on the lower linkage. In order to achieve a perfect plowing pattern under specific conditions, the AHC automatically controls the correct relationship between position and force by querying the sensor signals from the hitch. The tractor driver can also choose whether to drive in automatic mode.

This system can be activated and returned to manual mode at the press of a button or via CANbus. The Hitch Lowering Support (HLS) as an assist to the EHR also makes life simple for the operator. It enables pressure-assisted and thus rapid lowering of the hitch when the hydraulic fluid is cold, with or without implements. The defined pressure also makes unhitching easier, particularly for jammed catch hooks.

 

Search press releases


Contact

Melanie  Bright
15 Cromwell Road  
PE19 2ES Cambridgeshire
Phone: 01480 223 290
press@boschrexroth.co.uk

Related Articles

2016-11-30
Press Release

Silence is golden: New development in low-noise gear pumps for mobile applications

Diesel exhaust and noise pollution is an increasing concern for businesses, but for the agricultural sector it has always been an issue. Hydraulic systems have many applications and benefits, but few people would associate their use with a quiet working environment, until now.


2014-06-24
Product Information

Industry warned of grey repair threat to hydraulic and electronic drives

Non-official or ‘grey’ repairs to hydraulic and electronic drives are threatening industrial productivity by increasing downtime and placing warranties at risk, according to one of the UK’s leading drives and controls manufacturers.