How Bosch Rexroth's Hydraulic Solutions Are Paving the Way
Have you ever wondered how rainwater is diverted away from our city during heavy downpours? The answer lies beneath the bustling streets of Kuala Lumpur, where the innovative Stormwater Management and Road Tunnel (SMART tunnel) plays a dual role in combating floodwaters and easing traffic congestion. We, Bosch Rexroth, are proud to be a driving force behind this transformative project. Here is an inside look at how our products and solutions are revolutionizing Kuala Lumpur's urban resilience.
Heavy rainfall during monsoon seasons and the relentless work-hour rush are common woes for residents of Kuala Lumpur. The city's topography, coupled with the intensity of rainfall, often leads to flash flooding that disrupts daily life and poses a significant threat to infrastructure. Local officials recognized that a drainage tunnel, which was proposed to prevent the city's rivers from flooding during heavy rains, could also help ease traffic congestion.
This resulted in the 9.7 km SMART tunnel, which serves two purposes: it reduces the city's flash flooding and rush-hour traffic congestion. Flood water from a heavy downpour is routed through the bypass tunnel beneath the motorway tunnel. The motorway tunnel is closed to traffic if flooding worsens and rains continue, allowing water to flow through both the traffic and bypass tunnels. Bosch Rexroth's hydraulic systems play a pivotal role in this symphony of flood management by seamlessly controlling SMART tunnel gates, ensuring efficient flood protection.
According to the calculations made by the Department of Irrigation and Drainage Malaysia, the total cost of damage caused by the floods along the SMART tunnel alignment was estimated to be around RM 20.2 million. The tunnel mitigates 45% of the major floods in the Klang Valley alone, making it a beacon of urban development and a model for other developing nations to follow, especially in the context of climate change adaptation. Source
So, where do we come in? Closing the tunnel to traffic only happens during major storms. Floodgates seal it off at each end, and water from Kuala Lumpur's rivers is pumped through to prevent them from breaking their banks. We partnered with government authorities and contractors to upgrade the drive and control systems of radial gates in Kampung Berembang pond, a holding basin with a massive water volume. Our hydraulic systems involvement operates water gates in three crucial ponds in Kuala Lumpur and the SMART tunnel.
One remarkable enhancement by Bosch Rexroth lies in the coordination of Hydraulic Power Units (HPUs). Initially, each gate had its dedicated HPU, but they could not communicate with one another, potentially leading to inefficiencies during emergencies. Our proposed solution now allows each HPU to manage multiple gates, improving the tunnel's flood management capabilities. Each gate is assigned to a dedicated Hydraulic Power Unit. These HPUs use hydraulic fluid to generate the necessary pressure and force required to open and close the gates. When there is a risk of flooding, the HPUs are activated to close the gates, preventing water from entering the city center through the tunnel. The hydraulic system used in the SMART tunnel is critical for the tunnel's flood mitigation capabilities. It allows for efficient and precise control of the gates, ensuring that the tunnel can swiftly respond to changing weather conditions and potential flood threats. The use of hydraulics in this context provides a reliable and robust method to manage water flow and protect the city from flooding.
Another remarkable project involving Bosch Rexroth's hydraulic expertise is the link between the SMART tunnel and the Tun Razak Exchange (TRX) connection. The SMART tunnel, directly linked to the TRX underground parking space, can accommodate 5,000 cars and has been built to boost the upcoming international business district connectivity. In this endeavor, Bosch Rexroth's hydraulic cylinders play a pivotal role in controlling the floodgates at TRX. The synchronized operation of these gates, expertly managed by Bosch Rexroth's technology, ensures effective flood mitigation during high water levels, contributing to a more resilient city.
Why choose Bosch Rexroth's hydraulic solutions for such critical projects? The answer lies in the core principles of safety and reliability. Our Hydraulic Power Units (HPUs) and Hydraulic cylinders offer consistent performance even in the most challenging conditions, safeguarding urban areas from potential disasters. Moreover, our commitment to Industry 4.0 compatibility positions us at the forefront of modern hydraulic solutions. Our systems are designed for data collection, remote monitoring, and predictive maintenance - crucial elements in the smart cities of the future. By enhancing efficiency, reducing risks of accidents, and embracing the principles of Industry 4.0, our solutions are not only improving infrastructure but also paving the way for greener, smarter urban planning.
In closing, Bosch Rexroth's hydraulic solutions are at the forefront of revolutionizing Kuala Lumpur's urban landscape. As we stand shoulder-to-shoulder with the city in its journey towards a smarter, more resilient future, we are reminded that the fusion of technology and infrastructure is the cornerstone of sustainable urban development. As the Kuala Lumpur skyline continues to evolve, it does so with the assurance that its infrastructure is not just equipped for today but primed for the challenges of tomorrow. Bosch Rexroth remains committed to paving the way for a brighter and more resilient future for Kuala Lumpur and beyond.