1. Home
  2. Blog
  3. AT
  4. Aluminum Framing - Data Center Construction (US)
Aluminum Framing as the Backbone of a Successful Data Center Construction
Aluminum Framing as the Backbone of a Successful Data Center Construction
Assembly Technology

Aluminum Framing as the Backbone of a Successful Data Center Construction

In an AI-driven shift, data center construction is growing at a rapid pace.

In 2025, the data center construction market was estimated at 261 billion and expected to steadily grow at a 12% CAGR through 2033.

To meet the demand, additional data centers need to be built with speed and longevity in the forefront. After all, a data center malfunctioning can be detrimental. That’s why a successful data center needs to be built correctly – before the servers even enter the building.

A Tale of Two Materials: Steel and Aluminum

In the high-stakes world of data centers, where every degree of temperature matters, installation efficiency and overall reliability are paramount.

While steel is often viewed as the preferred material due to its strength and structural integrity, this emphasis on efficiency and reliability give aluminum framing its edge. Compared to steel, aluminum framing is more lightweight for easier handling, boasts a stronger strength-to-weight ratio, and greater thermal conductivity.

When purchased in bulk for a large project like constructing a data center, aluminum framing is often more economical, and quicker for construction workers to handle in installation due to being lighter.

Depending on the application, both steel and aluminum can often work together for the overall build. Steel does greater load-bearing strength and if the weight requirements extend aluminum’s specification, using steel is a solution. But in key data center applications like hot aisle containment, cold aisle containment, false floors, and even server racks, aluminum framing is a smart start to a successful data center.

Top Aluminum Framing Applications in Data Center Construction

While aluminum framing can be used in more applications, the strengths of the material shine brightest with the following applications:

  • Hot Aisle Containment
  • Cold Aisle Containment
  • Server Racks
  • False Floors

Hot Aisle Containment

Temperature management is a critical consideration for data centers. Hot aisle containment systems are paramount to reduce energy consumption and improve overall efficiency by preventing the mixing of hot exhaust air and cold supply air. With its ability to form an air-tight containment seal, thermal-conductivity benefits, and easy installation, aluminum framing is the ideal material structure for these critical enclosures.

With a modular aluminum framing system, it can also adapt and be reconfigured if the data center needs to shift as technology evolves.

Cold Aisle Containment

Cold Aisle Containment encloses the aisle where cold supply air is supplied to equipment, using panels and doors to separate it from hot exhaust air. All the same benefits of aluminum framing from hot aisle containment apply to this application.

Server Racks

Beyond aisle containment and temperature control, aluminum profiles are revolutionizing server rack construction. Steel racks will be heavy, which makes them hard to move and limits their adaptability. Aluminum profiles, however, offers a superior alternative that are not only incredibly strong but also remarkably light, facilitating easier transportation and deployment.

False Floors

Data centers require raised floors, also known as false floors, that are elevated between 1-2 feet and support cable management, as well as a distribution system for cold air to server racks. With its impressive strength-to-weight ratio and easier installation, aluminum framing makes an efficient material for false floors that improve cooling efficiency by supporting underfloor airflow.

Beyond its technical strengths, aluminum framing provides unmatched aesthetics - clean lines, precision surfaces, and modularity create an impressive environment that is not just functional, but visually impressive. In a rapidly changing market, where efficiency, speed, and precision are paramount, a material solution that looks as sleek as it performs speaks volumes about the quality of the entire infrastructure.