When you are engineering a massive industrial press, a die-casting machine, or a primary metal processing line, your focus is naturally on raw power. You need to move heavy loads with immense force, which means specifying hydraulic valves capable of handling massive flow rates and high pressures.
But as any veteran machine builder knows, specifying the hydraulics is only half the battle. The real headache usually starts when it’s time to wire it all together.
Traditionally, controlling a high-flow proportional valve meant dealing with a disconnected system. The "muscle" (the valve itself) lived out on the harsh factory floor, while the "brain" (the amplifier card) had to be safely tucked away in a central electrical cabinet.
Connecting the two created a logistical nightmare. You had to carve out valuable real estate in the control panel for the amplifier cards. Then, your team had to run long, expensive, shielded multi-core cables across the machine to connect them. Not only did this drive up material costs and labor hours, but those long analog cable runs were highly susceptible to electrical noise and signal degradation, making troubleshooting a frustrating game of hide-and-seek.
It was standard practice, but it was never truly efficient.
Bosch Rexroth engineered the 4WRZE pilot-operated proportional valve to eliminate this disconnect. By utilizing advanced On-Board Electronics (OBE), we’ve taken the amplifier out of the control cabinet and integrated it directly onto the valve body itself.
It’s the same proven Rexroth hydraulic muscle, but with a built-in brain. Here is how this integrated approach transforms machine design:
Upgrading to the 4WRZE with OBE is more than just swapping a component; it’s an opportunity to completely streamline your machine's electrical architecture.
Because the amplifier is already on the valve, you can permanently cross external drive cards off your bill of materials. Your control cabinets can be significantly smaller, saving premium floor space and reducing enclosure costs. Furthermore, commissioning speeds up dramatically. Instead of pulling shielded analog cables and terminating dozens of tiny wires, your team simply plugs in a standard industrial connector.
If an issue ever does arise, maintenance is straightforward. There is no need to trace a signal from a dirty machine back to a crowded panel—the entire valve and control unit can be diagnosed or swapped as a single, accessible package.
You shouldn't have to build a bigger electrical cabinet just to get more hydraulic flow. The 4WRZE proportional valve gives you the immense power your application demands, with the integrated simplicity your engineering team deserves.
Ready to streamline your next heavy-duty build? Contact a Bosch Rexroth specialist today to see how On-Board Electronics can transform your system design.