Edge Edition for enhanced cobot mobility
With its Edge Edition cobots, Kassow Robots has miniaturized the robot controller to about 10 percent of its original size and launched the world’s first 7-axis cobots in which the controller is integrated into the base of the robot. In this interview, founder and CEO Kristian Kassow talks about the advantages of this innovation.
Kristian Kassow: Our goal has always been to make it as easy as possible for our customers to integrate cobots into their production, with an explicit focus on SMEs. Our Edge Edition offers multiple advantages here: it’s designed for industrial use, offers a high level of maneuverability thanks to its 7 axes, and delivers unique compactness. It also has a small footprint of just 160 x 200 millimeters. That is because we have miniaturized the controller to just 10 percent of the original size and integrated it into the robot base. Another benefit worth mentioning is that the Edge Edition can be easily connected to any DC power supply, such as the battery of a mobile robot.
Kassow: Lots of them, all industries with intralogistics tasks at their production sites can benefit from our Edge Edition! The Edge Edition offers the additional benefit of being a multifunctional cobot, allowing users to switch between tasks seamlessly. This includes the ability to use it for the production of Product A, followed by a quality check, and then for palletizing. The Edge Edition comes into play and shows off its advantages when a cobot becomes an efficient assistant to mobile robots.
Kristian Kassow: “We believe that mobile applications will be the primary use for the Edge Edition. This means using cobots in combination with an AMR or AGV.”
Kassow: One way in which the cobot can be made mobile is by moving the lightweight cobot installation to a new location and programming it for a new application. The programming of a cobot is much easier than in the case of a traditional industrial robot. Another way to make the most of mobility is to use it for the same tasks that come up at various locations during the production process. Let me give you an example. A combination of an AGV/AMR and a cobot can take over the task to take care of the loading of boxes which will be used for packaging.
Kassow: To summarize: The Edge Edition saves space because the robot arm and controller form a compact unit that can be installed quickly. In addition, as mentioned earlier, the direct current (DC) connection on all Edge Edition cobots satisfies all the requirements for connecting a cobot directly to the battery of an AGV or AMR. At the end of the day, we want to make it easier for our customers to integrate cobots into mobile solutions.
A look at today’s AGVs and AMRs quickly reveals just how little space they offer. Robot controllers are mostly bulky, making it harder to automate tasks. Our Edge Edition cobots feature a slim base. We help system integrators and end customers simplify the implementation of these AGV/AMR & cobot solutions.