USA

Select your location

USA
 

Press

Content
xxx 2013-09-23

Productive Pneumatic Solutions for the Food and Packaging Industry

Productive Pneumatic Solutions for the Food and Packaging Industry

Rexroth develops hygienically designed pneumatic components – for automation and handling.

Specially designed for use in the food and packaging industry, pneumatic components from Rexroth enable hygienic handling of food products and efficient packaging of all types of workpieces. Whether grippers, cylinders or valve terminal systems: all components in this range are perfectly matched and can be combined according to the special requirements of food processing as well as primary, secondary, or end packaging needs.


In the food sector, the processing and packaging of foodstuffs is subject to strict hygiene requirements. Products are processed, positioned, picked up by grippers, placed in the packaging provided by handling portals and sent further down the line or packaged. All these steps must take place under hygienic conditions. As a result, the main prerequisites for machine components are robust materials and ease in cleaning, with smooth surfaces and no seams or hard-to-reach areas. Hygienically designed pneumatic components from Rexroth meet the highest hygiene standards, even in the wet areas of systems.


Hygienic design was therefore a top priority in the development of the CL03 valve terminal system, which has meanwhile been awarded EHEDG certification. The features of the valve terminal system, designed in accordance with protection class IP69K, permit direct installation in production facilities, eliminating the need for a separate control cabinet.


The corrosion-resistant ICS-D1 ISO cylinder made of acid-proof steel is recommended particularly for applications in food processing. All types of fluid, right up to aggressive acids, can be easily washed off these hygienically designed round cylinders. The cylinder is also available in a heat-resistant version with special seals.


For wash-down applications, the guide cylinders in the GPC Clean series are the right choice. Their housing is made of anodized aluminum, which stands up to extremely harsh cleaning processes. The front plate and screws are manufactured from stainless steel. The smooth surface is free of grooves and holes, thus facilitating cleaning.


With the NCT transport system from Rexroth, which operates according to the Bernoulli principle, porous or air-permeable objects, as well as soft materials or highly sensitive workpieces, can be easily and gently lifted and transported. In addition to the aluminum version for general handling functions, the NCT is now also available in PEEK. The properties of the FDA and EC-approved material, i.e. resistance to chemicals, conventional solvents, acids, salts and oil, fulfill the requirements of the food industry. They guarantee the safe use of these components, even when in direct contact with food products. A low friction coefficient and high resistance to wear ensure a long service life and hygienic handling.


For an optimum connection of the pneumatic components, even under the harshest conditions, Rexroth also offers acid-proof accessory parts, including fittings.


For a list of specifications as well as available features and accessories please visit www.rexrothpneumatics.com/us


About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, pneumatics, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 37,500 associates generated sales revenue of approximately 6.5 billion euros ($8.4 billion) in 2012.

To learn more, please visit www.boschrexroth-us.com


About Bosch:

The Bosch Group is a leading global supplier of technology and services, active in the fields of automotive technology, energy and building technology, industrial technology, and consumer goods. According to preliminary figures, more than 306,000 associates generated sales of 52.3 billion euros( $67.2 billion) in 2012. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some 4.5 billion euros ($5.8 billion) for research and development in 2012, and applied for over 4,700 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at www.bosch.com and www.bosch-press.com


In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software solutions. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011. For more information, please visit www.boschusa.com, www.bosch.com.mx and www.bosch.ca.

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com