USA

Select your location

USA
 

Press

Content
xxx 2013-09-23

Valve system for applications in wet areas

Valve system for applications in wet areas

Compliant with IP69K: CL03/CL03-XL valve system in hygienic design.

Designed for protection class IP69K and certified by EHEDG, the CL03 valve system can be installed directly in systems for the food processing industry, thanks to its design and the material properties. A separate control cabinet is not required. With the new CL03-XL version, the system is now available with a high flow rate of 1100 l/min for use with larger actuators. Its special plus: different valve sizes can be combined in the same unit. Rexroth thus enables different flow rates in a single valve unit with a hygienic design.


With the CL03-XL variant of the CL03 valve system, operators can control larger cylinders or actuators for faster movements, without having to install a dedicated valve unit or separate individual valves for the larger consumer. The key is a uniform base plate where different valve sizes can be integrated at any position. There is no need for adapter plates, as the position and geometry of the air channels are identical in all valves, independent of their size. This reduces the installation effort. Users also profit from the design with integrated combination options, which requires just one control.


When only one valve unit is used instead of many, cleaning is a lot simpler. In wet areas of a system in particular, units have to be not only compact but also especially suitable for fast and thorough cleaning. The fewer the components, the easier the cleaning. A single valve unit with different flow rate options, such as CL03/CL03-XL, is the ideal solution for such situations. Another advantage: tubing from the valve to the actuator stays as short as possible, and there is no unnecessary dead volume. That saves energy. The CL03-XL valve system can implement up to 32 pressure zones and is available with multipole or field bus interface. The electrical signal can be tapped directly and put to further use.


The CL03/CL03-XL valve system's modular design and special materials have successfully withstood tests to measure resistance to a wide range of cleaning chemicals. The valve housing was designed in line with hygienic criteria to avoid joints, slots, or gaps. Classified in the high protection class IP69K, this valve system is ideal for cleaning at high pressure and high temperatures. Dirt deposits and related risks of contamination can thus be avoided. As a result, the system can even be used in areas where direct contact with food products is an issue.


For a list of specifications as well as available features and accessories please visit www.boschrexroth-us.com


About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, pneumatics, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 37,500 associates generated sales revenue of approximately 6.5 billion euros ($8.4 billion) in 2012.

To learn more, please visit www.boschrexroth-us.com


About Bosch:

The Bosch Group is a leading global supplier of technology and services, active in the fields of automotive technology, energy and building technology, industrial technology, and consumer goods. According to preliminary figures, more than 306,000 associates generated sales of 52.3 billion euros( $67.2 billion) in 2012. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some 4.5 billion euros ($5.8 billion) for research and development in 2012, and applied for over 4,700 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at www.bosch.com and www.bosch-press.com


In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software solutions. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011. For more information, please visit www.boschusa.com, www.bosch.com.mx and www.bosch.ca.

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com