USA

Select your location

USA
 

Press

Content
xxx 2013-09-19

Distributed drives for streamlined automation

Distributed drives for streamlined automation

The advanced motor integrated IndraDrive Mi: The integrated Motion Logic system controls up to ten axes without a superordinate control system

IndraDrive Mi from Rexroth with drive-integrated Motion Logic.


In theory, the most economic value added chain in machinery construction is something that has long been known: pre-assembling stand-alone machine modules in series and only making decisions regarding functions and command communications in the software immediately prior to installation. Rexroth now provides the technology needed for that ideal with its advanced motor-integrated IndraDrive Mi drives. The drive-integrated Motion Logic system controls up to ten axes without a superordinate control system. The Multi-Ethernet interface supports all established real-time Ethernet protocols. The new drive-integrated safety functions allow machine manufacturers to divide the drives involved standardized into safety zones.


The advanced distributed IndraDrive Mi servo drives independently perform logic and motion tasks based on IEC 61131-3 thanks to the integrated Rexroth IndraMotion MLD. One master drive controls up to nine slave drives in hard real time via the Sercos automation bus. The automation also integrates Ethernet actuators and peripheral devices directly connected to the drives, allowing users to pre-assemble complete modules without control cabinets and thereby reducing necessary wiring by up to 85%.


The new Multi-Ethernet interface standardizes hardware independent of the command communication used. Configuration of the Sercos, PROFINET IO (RT), EtherNet/IP, and EtherCAT communication protocols is executed exclusively via the software, giving machine manufacturers the flexibility to adapt pre-assembled series modules to individual machine versions with different communication architectures. A communication cord is all that is needed for connection to the superordinate control system or other modules.


The distributed Safe Torque Off (STO) Safety on Board function also offers enhanced modularization options. When the STO function is activated, the drive interrupts the torque and field-forming current to the connected motor within a few milliseconds without a detour via the control cabinet and superordinate control system. The STO function in the IndraDrive Mi is certified with Kat 4 PL e pursuant to EN ISO 13849-1 and SIL 3 pursuant to EN 62061. Users can simultaneously activate torque connection for all connected drives using simple wiring. Alternately, users can also create various safety zones with the needed number of IndraDrive Mi, thereby creating specific safety zones for individual unit modules. The other modules can continue to work without interruption while the activated STO function ensures standardized security for manual procedures.

For a list of specifications as well as available features and accessories please visit www.boschrexroth-us.com


About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, pneumatics, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 37,500 associates generated sales revenue of approximately 6.5 billion euros ($8.4 billion) in 2012.

To learn more, please visit www.boschrexroth-us.com


About Bosch:

The Bosch Group is a leading global supplier of technology and services, active in the fields of automotive technology, energy and building technology, industrial technology, and consumer goods. According to preliminary figures, more than 306,000 associates generated sales of 52.3 billion euros( $67.2 billion) in 2012. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some 4.5 billion euros ($5.8 billion) for research and development in 2012, and applied for over 4,700 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.”

Additional information is available online at www.bosch.com and www.bosch-press.com


In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software solutions. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011. For more information, please visit www.boschusa.com , www.bosch.com.mx and www.bosch.ca .

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com