USA

Select your location

USA
 

Press

Content
xxx 2013-02-10

Rexroth Introduces Open Core Engineering

Rexroth Introduces Open Core Engineering

With the Open Core Interface OEMs can develop application programs with Java as native apps and integrate smartphones seamlessly into the automation process.

Bosch Rexroth is introducing an innovative approach to connect PLC and IT automation that it calls Open Core Engineering, the platform gives developers a greater degree of freedom in software engineering. OEMs can flexibly access the control core of the system solutions IndraMotion MLC and IndraLogic XLC from applications based on high-level languages. This allows them to realize customized solutions independently and more easily, and at a lower cost than before.


Open Core Engineering brings the requirements from previously separated engineering worlds together in one integrated solution. At its center are software tools and function toolkits that build entirely on open standards and technologies. The new Open Core Interface enhances the software engineering – which until now has been focused on PLC automation – enabling it to work with applications based on high-level languages. With numerous function libraries which are adapted to different development environments it is now possible to have functions directly access the control core. This allows OEMs to realize customized software functions in-house and to integrate IT technologies based on high-level languages into their automation solutions. Specific examples are the integration of simulation tools or the use of smart devices with native apps. Moreover, the Open Core Interface makes it possible to integrate production machine functions and data out of IT-based applications such as management execution systems.


Access all the way to the core with various devices and programming languages

With the Open Core Interface, OEMs are free to choose their platform – PC, controller or smart device – and the required programming language: From C/C++, C# (.NET), Visual Basic, VBA (Office), LabView G, Objective-C and Java to all programming applications that support the integration of Microsoft COM libraries. They can even realize customized control functions for real-time applications independently of the control program. This means that the engineers can use high-level languages to write their own software functions which then run as low-level real-time application directly on the control, or in non-real-time on external devices such as PCs or smart devices. Now machinery manufacturers can realize innovative functions themselves - even those that require enhanced core access. This will also allow them to protect their know-how.


Smart devices and native apps as application examples

The Open Core Interface supports Apple iOS and Google Android, which are the two major operating systems for smartphones and tablets at this point. The high market penetration of smart devices combined with their innovative and comfortable operating concepts is generating a lot of interest with machinery manufacturers and operators. They are realizing that the future will bring new ways of making communication between humans and machines more user-friendly, flexible and intuitive. With the Open Core Interface, OEMs can develop application programs with Java as native apps, integrate smartphones seamlessly into the automation process, and support machine operators with new diagnostic and operating concepts. The native applications run entirely on the smartphone or tablet, so that the machine program remains untouched.


More efficient through integrated know-how

Open Core Engineering combines these new degrees of freedom in software engineering with engineering efficiency from project planning to ongoing operations, which is what the market had been demanding. The IndraWorks software integrates all tools as well as Rexroth's industry and technology-specific know-how in the form of function toolkits in an integrated engineering framework. The GAT (Generic Application Template) software toolkit, for instance, automatically generates the executable machine program based on the developer's instructions, thereby laying the foundation for the development of modular machine software. Another example is the FlexProfile software toolkit. It simplifies the execution of complex machine functions by automatically adjusting all drive movements to changed parameters in the production process.


A variety of industry and technology-specific software toolkits speed up the engineering as OEMs receive already pre-made basic functions. Based on open standards such as Sercos, OPC-UA or PLCopen, Open Core Engineering also provides certainty for the future and protects the investments of machinery manufacturers and operators.

For additional information, please contact info@boschrexroth-us.com


Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 38,400 associates generated approximately 6.4 billion euros ($8.9 billion) in revenue in 2011.

To learn more, please visit www.boschrexroth.com


The Bosch Group is a leading global supplier of technology and services. In the areas of automotive technology, energy and building technology, industrial technology, consumer goods, more than 300,000 associates generated sales of 51.5 billion euros ($71.7 billion) in 2011. The Bosch Group comprises Robert Bosch GmbH and roughly 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Each year, Bosch spends around 4.2 billion euros ($5.8 billion) for research and development, and applies for over 4,100 patents worldwide. The Bosch Group’s products and services are designed to improve quality of life through solutions that are innovative and beneficial, as well as fascinating. In this way, the company offers technology worldwide that is “Invented for life.” Additional information is available online at www.bosch.com and www.bosch-press.com


In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software solutions. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011. For more information, visit www.boschusa.com, www.bosch.com.mx and www.bosch.ca

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com