xxx 2012-12-05

New A15VSO high-pressure axial-piston unit from Rexroth with improved efficiency

New A15VSO high-pressure axial-piston unit from Rexroth with improved efficiency

New benchmark for ultra-low noise emissions: The A15VSO operates up to 3 dB(A) quieter than previously available high-pressure axial-piston pumps.

Rexroth combines significantly lower noise emissions with further improved efficiency in the new A15VSO axial-piston unit for stationary applications in open circuit operation. It can meet pressure requirements to 420 bar and recovers potential energy during pump/motor operation almost completely. This enables innovative recuperation concepts that can improve the efficiency of machines and systems. Equipped with a universal through drive, the A15VSO seamlessly integrates into the Rexroth line of products and simplifies the process of combining different pumps.

Rexroth developers used state-of-the-art simulation tools in all design stages. The housing structure, optimized for minimum sound emissions, reduces noise considerably. Subsequently, the air borne noise level has been reduced in average by up to 2 dB(A) at full flow operation and up to 3 dB(A) during pressure holding periods (high pressure stand by). In addition, the development engineers shifted the operating noise to a frequency range that is perceived as sonorous and more agreeable by the human ear.

Further design improvements increase the overall efficiency of the axial-piston pump to 93 percent. The swivel range, for example, has been increased to +/- 100 percent to enable complete over center operation and an extremely fast decrease of pressure. In the pump/motor operating mode an almost complete recuperation of potential energy is possible for instance during lowering of a load or braking of a moving mass. This opens up new opportunities for maximizing the energy efficiency of machines and systems, whereby the robust and stable swivel action ensures highly dynamic performance with reduced response times. The first pump size of the A15VSO has a displacement of 280 cubic centimeter at a nominal pressure of 350 bar and a maximum pressure of 420 bar.

The new compact housing, which features an optimized layout of flow channels and better use of installation space, simplifies the process of fitting the pump even in very tight spaces. The universal through drive increases flexibility for customized drive solutions and can easily be used to connect axial-piston, gear, and other hydraulic pumps out of the comprehensive line of Rexroth pumps. Numerous hydraulic and electric controllers (also for remote control operation) enable efficient, highly precise control of power, pressure, and flow as well as load-sensing functions.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 38,400 associates generated approximately 6.4 billion euros ($8.9 billion) in revenue in 2011.

To learn more, please visit .

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software innovations. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011, per preliminary figures. For more information, visit .

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Further information is available online at and .


Search press releases


Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670