Bosch Rexroth uses engineering rules-based programming and a wide range of components to create hydraulic power packs that bridge the gap between standard market and custom units.
Bosch Rexroth is helping customers design and build hydraulic power packs with competitive pricing and lead times with RexPak.
Rexroth’s new RexPak hydraulic power unit bridges the gap from standard market products to engineered-to-order, custom power units for a variety of industries from machine tool applications on the shop floor to marine and offshore work miles from land.
RexPak combines specific customer input with an unmatched choice of options and accessories to create unique hydraulic power packs without the cost or delay of custom engineering.
Rexroth takes customer-supplied data and combines it with rules-based software to design hydraulic power unit configurations with up to 200-gallon reservoirs, and providing power up to 75 HP and 65 GPM with operating pressures to 3200 PSI. Aditional RexPak options include a wide range of fixed and variable displacement pumps, pressure and/or return line filters, motor starters, water and air coolers, heaters, temperature and level switches and drip trays. A comprehensive documentation package specific to the customer’s particular power pack is available including a bill of material, general hydraulic schematic, 2-D general assembly drawing, 3-D model and data sheets for all components.
The streamlined process allows Rexroth to offer a range of power units–from stationary configurations to portable power pack–that are optimized to achieve the highest peformance with the smallest footprint possible. Each power pack includes quality Rexroth components that have been pre-selected and tested by the application engineering specialists. And, since components are in stock or have short lead times, power packs can be delivered to customers within four to eight weeks.
For more information, or to view a list of available features and accessories for RexPak units please visit www.boschrexroth-us.com/hydpowerunits .
Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 38,400 associates generated approximately 6.4 billion euros ($8.9 billion) in revenue in 2011.
To learn more, please visit www.boschrexroth-us.com .
In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software innovations. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011, per preliminary figures. For more information, visit www.boschusa.com .
The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Further information is available online at www.bosch.com and www.bosch-press.com .
Susan Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com