USA

Select your location

USA
 

Press

Content
xxx 2012-09-06

IMTS 2012: Sytronix variable speed hydraulic drives integrate easily

IMTS 2012: Sytronix variable speed hydraulic drives integrate easily

Energy efficient hydraulic drives use high-efficiency pumps and variable speed motors. These designs offer higher machine performance along with significantly reduced power consumption.

Along with the productivity of a machine, energy consumption is increasingly a factor in the purchase decision. A hydraulic drive using variable speed pump capabilities offers the potential of significant energy savings. This new technology can provide an OEM with a solution requiring minimal engineering effort and ease of implementation. Bosch Rexroth Sytronix variable speed hydraulic drives offer such a solution.


Machine drives must often perform a number of complex tasks. While there are many approaches to solve these tasks, design engineers look to solutions that can also save energy. Solutions should offer savings from the selection of components to the engineering design and start-up. Bosch Rexroth’s design experience can provide an integrated solution from one source: Sytronix drives. Sytronix drives from Rexroth combine high efficiency hydraulic pumps with state-of-the-art electric drives. In addition, control software, matched to the unique requirements of the machine, is implemented in a best-in-class controller. The hydraulic drive package provides the design engineer with an integrated, ready-to-install, pre-configured solution. Machine performance is optimized without having the machine designer bogged down in the details of the hydraulic drive.


When selecting a Sytronix drive designed for a specific machine task, Bosch Rexroth has the industry expertise needed to find the best solutions. For example, if a machine requires clamping or gripping, 14 drive systems using the FcP 5000 series are available. Using one of these solutions, F/V drives combined with high efficiency pumps provide demand-driven hydraulic power. For more demanding applications, such as plastic machinery and forming technology, Rexroth offers 47 pre-configured hydraulic drives in the SvP 7000 series. These drives provide a wide range of performance in five classes utilizing unique combinations of electric servo motors and high efficiency pumps. More than 80 drives in the DFEn 5000 product line offer solutions for axis drives requiring higher power. Combining an intelligent pump, unique to Bosch Rexroth, and electronic controls that regulate the pump’s displacement and drive motor speed, full four quadrant operation is obtained.


Using Bosch Rexroth Sytronix hydraulic drives can reduce power consumption by up to 80 percent, while maintaining the same level of productivity. Additionally hydraulic drive noise emissions can be reduced by up to 20 dB (A), cooling requirements are greatly reduced and the overall life of the hydraulic drive is increased.


For a list of specifications as well as available features and accessories please visit www.boschrexroth-us.com .


Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 38,400 associates generated approximately 6.4 billion euros ($8.9 billion) in revenue in 2011.


To learn more, please visit www.boschrexroth-us.com .


In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software innovations. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011, per preliminary figures. For more information, visit www.boschusa.com .


The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Further information is available online at www.bosch.com and www.bosch-press.com .


 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com