xxx 2013-10-09

Bosch Rexroth launches the world’s most powerful direct drive

Bosch Rexroth launches the world’s most powerful direct drive

The new Hägglunds CBM hydraulic motor from Bosch Rexroth creates powerful opportunities. Taking over from the tried-and-true Hägglunds Marathon motor, the Hägglunds CBM packs 50% more torque into a motor that is smaller and up to 50% lighter than its predecessor. That gives it the world’s highest torque-to weight ratio.

For Bosch Rexroth customers, the new motor opens up new possibilities. The Hägglunds CBM not only handles heavier workloads, but also takes up less space and places less weight on the drive shaft. This means that customer machines, and in some cases the facilities that house them, can be smaller, lighter and simpler.

The motor’s reduced installation requirements, combined with the higher productivity it allows, can mean lower overall investments and increased long-term revenue. An additional benefit is the unique operating advantages of a hydraulic direct drive: full torque from zero speed, protection from shock loads and four-quadrant operation.

Power for growing demands

The Hägglunds CBM motor was developed in direct response to customer requests. Greater power is increasingly needed in many industries, and it is a prerequisite for a number of new applications, such as wind and tidal energy. The Hägglunds CBM provides power for these applications and many others.

Based on the Hägglunds CB platform, the Hägglunds CBM has internal advances that allow it to supply 6000 Nm/bar of specific torque. “The Hägglunds CBM satisfies the toughest new demands on the market,” says Lars Andrén, one of the key members of the Hägglunds CBM development team. “With its introduction, we can provide the unique advantages of a hydraulic direct drive to a broader range of applications than ever before.”

Tested to meet high expectations

In replacing a successful and trusted motor like the Hägglunds Marathon, Bosch Rexroth has left nothing to chance. Many years of R&D have gone into the Hägglunds CBM, as well numerous hours of testing to verify performance and quality. In fact, the Hägglunds CBM has undergone more lab testing than any other Hägglunds motor.

A smooth transition to greater power

Those looking to upgrade from the Hägglunds Marathon will be pleased to know that direct retrofit kits are available. These make exchanging the motor both quick and simple in existing machines.

All customers, however, will benefit from the ease of installing the Hägglunds CBM, since it has splines that simplify attachment to the drive shaft. (Shrink-disc adapters are also available.) Retrofitted or newly installed, the Hägglunds CBM makes it easy to meet the growing need for power.

For more information on other Rexroth solutions and expertise, visit .

About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, pneumatics, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 37,500 associates generated sales revenue of approximately 6.5 billion euros ($8.4 billion) in 2012.

To learn more, please visit

About Bosch:

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket solutions, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software solutions. Having established a regional presence in 1906, Bosch employs nearly 24,600 associates in more than 100 locations, with consolidated sales of $10.6 billion in fiscal year 2012. For more information, visit , and

The Bosch Group is a leading global supplier of technology and services. In fiscal 2012, its roughly 306,000 associates generated sales of $67.5 billion. Since the beginning of 2013, its operations have been divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some $6.1 billion for research and development in 2012, and applied for nearly 4,800 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.” Additional information is available online at and .


Search press releases


Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670