xxx 2013-10-09

Traction and Control System for Tugboat Winches - Hydraulic and Electrical System Engineering

Traction and Control System for Tugboat Winches - Hydraulic and Electrical System Engineering

Source: Damen Shipyards Group

For Damen Shipyards, Bosch Rexroth developed and engineered both the hydraulic and electrical systems for the winches of a new tugboat. The Damen ASD Tug 3212 is a newly designed tugboat for assistance activities at offshore LNG and oil terminals and open sea loading stations for the mining industry. The tug has 85 t Bollard Pull, a speed of 14 knots and two deck-mounted winches: one at the bow and one at the stern.

The winches are directly driven by the second-largest motor from the Hägglunds CB series. This compact and low-speed hydraulic motor features a low mass moment of inertia, high torque and minimal servicing needs.


The complete project comprised the pump sets, manifold blocks, motors, system controller, control cabinets and operator panels. Because Bosch Rexroth developed all the hydraulic and electrical systems needed – where they used proven components and technologies – the final solutions have a very compact design.

Other features of the systems are a low servicing need, the use of a closed loop system (that means a pre-set amount of energy can be returned to the system) and a special control feature that ensures that the line from winch to towed ship stays under tension. All the HMI (Human Machine Interface) and bridge components employ a modern touchscreen.

Single point of contact

Because Bosch Rexroth – as a system and development partner – engineered both the hydraulic and electrical systems, Damen had a single point of contact for an important part of the vessel. This prevented unnecessary discussions and reduced the development time.

About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, pneumatics, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 37,500 associates generated sales revenue of approximately 6.5 billion euros ($8.4 billion) in 2012.

To learn more, please visit

About Bosch:

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket solutions, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software solutions. Having established a regional presence in 1906, Bosch employs nearly 24,600 associates in more than 100 locations, with consolidated sales of $10.6 billion in fiscal year 2012. For more information, visit, and

The Bosch Group is a leading global supplier of technology and services. In fiscal 2012, its roughly 306,000 associates generated sales of $67.5 billion. Since the beginning of 2013, its operations have been divided into four business sectors: Automotive Technology, Industrial Technology, Consumer Goods, and Energy and Building Technology. The Bosch Group comprises Robert Bosch GmbH and its roughly 360 subsidiaries and regional companies in some 50 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some $6.1 billion for research and development in 2012, and applied for nearly 4,800 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.” Additional information is available online at and


Search press releases


Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670