xxx 2013-05-03

Bosch Rexroth highlights innovative solutions for offshore applications at OTC 2013

Bosch Rexroth highlights innovative solutions for offshore applications at OTC 2013

To view the press kit for OTC 2013 click here .

Comprehensive range of products and applications on display demonstrate expertise in offshore and marine technology

  • special vessel lifts offshore platforms in one piece
  • continuous jacking systems aid offshore wind installation
  • standard components adapted for deep sea applications
  • new surface technology for large hydraulics cylinders

Thanks to its worldwide application expertise and comprehensive research and development activities, Bosch Rexroth offers components and system solutions for offshore support vessels, exploration and drilling, offshore wind installation and deep sea applications. Several of those technologies will be on display at the Offshore Technology Conference, May 6-9, in Houston, TX, booth #5447.

Topside Lifting System reduces cost, increases safety in decommissioning platforms

As the major engineering partner to the Allseas Group, Bosch Rexroth has developed and engineered the drive and control system solution for the world’s largest mobile lifting mechanism for offshore installations. The special vessel equipped with this topside lifting system (TLS), “Pieter Schelte,” can lift and transport topsides of offshore platforms with a weight of up to 48,000 tons in one piece.

To disassemble topsides of offshore platforms, workers used to have to manually disassemble the structure into transportable individual parts on the high seas – work that is both time consuming and hazardous. In the future, the new special vessel from the Allseas Group will completely lift the platforms from their steel “jacket” and transport them onto land, making disassembly considerably safer and more cost-effective.

Continuous jacking systems for increased productivity and safety

The market for wind energy puts challenging additional demands on traditional jacking systems for installation and maintenance vessels and platforms. Bosch Rexroth meets the latest demands with a new standard in jacking: the high performance continuous jacking system. Besides the increasing the load capacity, working at higher jacking speeds, and an advanced control system, specifically integrated features lead to more reliability, safer operations and a considerable reduction of required power.

The jacking cylinders are equipped with CIMS (Cylinder Integrated Measuring System), which provides a most accurate signal required by the control system to evaluate the status of the system in relation to the precision, motion pattern and leveling of the vessel or platform. The cylinder rods are protected by a surface technology that is suitable for harsh environment conditions.

And a modern operator will benefit from a tight integration of the jacking system with the crane, mooring, handling and sea fastening systems. This integration adds to the redundancy and reliability of the vessel and to interesting cost savings. Secondary controlled drive systems for the vessel crane combine high performance with reduced power consumption, occupied space and weight.

Standard components adapted for deep-sea applications

Rexroth is the first to adapt numerous standard components to fit the special requirements for deep-sea applications such as pressure compensation and corrosion protection to provide equipment with a longer maintenance-free life span and optimal performance.

In order to test its designs, Rexroth developed a Subsea test power unit equipped with a water-proof motor/pump assembly that can drive an axial piston motor and hydraulic cylinders via an encapsulated valve control. The hydraulic system comes in a pressure-compensated design. Rexroth tested the equipment in a unique pressure chamber facility, was able to demonstrate suitability of its hydraulic components to a depth of 6,000 meters below sea level.

Enduroq 3200: Surface Technologies for Large Hydraulic Cylinders

Large hydraulic cylinders are used in many offshore applications, like riser tensioning, heave compensation, skidding, deck mating and jacking. The piston rod surface of these engineer-to-order products is one of the most essential parts of the hydraulic installation.

With more than 50 years of experience and service data feedback from the largest installed cylinder base in the world, Rexroth now offers Enduroq 3200 as an extension of its existing in-house technologies for piston rods of large hydraulic cylinders. These solutions include the existing Enduroq 3000, a single layer Ultimet based surface technology, and Enduroq 2000 and Enduroq 2200, both based on the proven HVOF technologies.

About Bosch Rexroth:

Economical, precise, safe, and energy efficient: drive and control technology from Bosch Rexroth moves machines and systems of any size. The company bundles global application experience in the market segments of Mobile Applications, Machinery Applications and Engineering, Factory Automation, and Renewable Energies to develop innovative components as well as tailored system solutions and services. Bosch Rexroth offers its customers hydraulics, electric drives and controls, pneumatics, gear technology, and linear motion and assembly technology all from one source. With locations in over 80 countries, more than 37,500 associates generated sales revenue of approximately 6.5 billion euros ($8.4 billion) in 2012. To learn more, please visit .

About Bosch:

The Bosch Group is a leading global supplier of technology and services, active in the fields of automotive technology, energy and building technology, industrial technology, and consumer goods. According to preliminary figures, more than 306,000 associates generated sales of 52.3 billion euros( $67.2 billion) in 2012. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent some 4.5 billion euros ($5.8 billion) for research and development in 2012, and applied for over 4,700 patents worldwide. The Bosch Group’s products and services are designed to fascinate, and to improve the quality of life by providing solutions which are both innovative and beneficial. In this way, the company offers technology worldwide that is “Invented for life.” Additional information is available online at and

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software solutions. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011. For more information, please visit, and


Search press releases


Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670