USA

Select your location

USA
 

Press

Content
xxx 2012-09-18

MINEXPO 2012: Torque Arm Drive System (TADS) from Bosch Rexroth delivers high performance and high reliability

MINEXPO 2012: Torque Arm Drive System (TADS) from Bosch Rexroth delivers high performance

Rugged, reliable and versatile, the Hägglunds TADS hydraulic drive system from Bosch Rexroth is a powerful, self-contained drive package for applications and systems where space is at a minimum.

The Hägglunds TADS unit represents maximum performance in smallest footprint possible by creating a self-contained drive package where the torque arm serves as the framework for mounting the complete drive system.

This allows the TADS unit to occupy approximately the same space as a normal low speed, high torque motor with torque arm mounting, but eliminates the external equipment such as gearboxes or heavy pedestal foundation elements, which are no longer required. This means that customer machines, and in some cases the facilities that house them, can be smaller, lighter and simpler without sacrificing the power to handle heavier workloads making the TADS system a great hydraulic drive system for industries like mining and bulk materials handling.

The TADS unit offers machine designers the flexibility to integrate the power of Hägglunds hydraulic drives into the widest range of industrial applications by offering nine different modular configurations with both spline and shrink disc coupling options.

Easy to install and use

The TADS unit comes preassembled and ready to mount on the process machinery’s drive shaft, saving installation time and costs. It can be installed using either an internal spline or hollow shaft with shrink disc couplings -- and none of the extra hoses or control cabling typically required with a conventional power unit and motor.

All Hägglunds motors and drives are engineered to deliver maximum torque from zero speed with infinitely variable settings. Plus, they are manufactured to deliver high reliability and long service life, protection from shock loads and operation of infinite start, stop and reverse that does not damage the system.

The Hägglunds TADS unit features extremely fast hydraulic pump compensators that can reduce the wear and lengthen the life of any machine. Load-sensing and power-limiting tools enable operators to intelligently sustain peak levels of operation that outperform other systems -- boosting machine uptime and helping reduce total cost of ownership.

For more information on other Rexroth solutions and expertise, visit www.boschrexroth-us.com/.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 38,400 associates generated approximately 6.4 billion euros ($8.9 billion) in revenue in 2011.

To learn more, please visit www.boschrexroth-us.com.

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software innovations. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011, per preliminary figures. For more information, visit www.boschusa.com.

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Further information is available online at www.bosch.com and www.bosch-press.com.

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com