xxx 2011-05-17

Lower the boom on fuel usage and component costs

Lower the boom on fuel usage and component costs

Thanks to gravity, “Green Valves” from Rexroth reduce fuel consumption and increase boom function performance on cranes, telehandlers and other mobile equipment.

Rexroth introduces a new concept in load-holding and lowering valves to make mobile equipment more energy efficient and easier to control. Using the force of gravity instead of engine power to help lower a boom, Rexroth’s new "Green Valves" dramatically decrease power requirements, thereby saving fuel and cutting emissions.

Rexroth’s new Green Valves all but eliminate the need for energy consuming high pressure and high oil flow. Engineered to replace traditional counterbalance valves, the patent-pending design allows the use of gravity to help lower the loaded or unloaded boom, while at the same time providing increased stability and control. This results in quicker boom movement and also smoother starting and stopping action. In addition, the Green Valves barely require any oil flow to lower the boom so more oil flow is available for faster execution of other simultaneous movements. This can further shorten machine cycle times for better performance.

By drastically reducing the energy required from the diesel engine to lower the boom, the new load-holding valves can provide significant fuel savings and also help in meeting emission standards. Higher fuel savings result in a more sustainable use of resources, which led to the product name, Green Valves.

The high level of stability and controllability integrated into the valves eliminates the need for damping devices such as orifices, thereby saving costs and also valuable installation space.

Suitable for any type of hydraulic circuit, Rexroth’s Green Valves are compact, easy to install, and interchangeable with current Rexroth counterbalance valves.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the brand name of Rexroth the company supplies more than 500,000 customers with tailored solutions for driving, controlling and moving machinery used in industrial and factory automation as well as in mobile applications. Bosch Rexroth is a partner for industrial applications, factory automation, mobile applications and renewable energy development. As The Drive & Control Company, Bosch Rexroth develops, produces and sells components and systems in more than 80 countries. In 2008 Bosch Rexroth AG, part of the Bosch Group, achieved sales of around $8.3 billion (5.9 billion Euro) with 35,300 employees. Visit for more information.


Search press releases


Bosch Rexroth  Corporation
Prairie Stone Parkway 5150
60192 Hoffman Estates, IL
Phone: (847) 645-3728
Fax: (847) 645-3728