USA

Select your location

USA
 

Press

Content
xxx 2011-09-20

AATExpo 2011: Miniature 10mm and 15mm Pneumatic Valves

AATExpo 2011: Miniature 10mm and 15mm Pneumatic Valves

The modular line of 3/2 and 2/2 miniature direct-acting valves with 10mm and 15mm valve body widths feature fast response, with a high flow rate, at an economical price.

The DO10-BMR and DO15-MR series miniature pneumatic directional control valves from Rexroth have many features in a compact package. The DO10-MR (10mm valve body width) has a flow rate of 0.014Cv, and the DO15-MR (15mm valve body width) has a flow rate of 0.05Cv.

(Lexington, KY – www.boschrexroth-us.com/brp ) The DO10-MR and DO15-MR are direct-acting, solenoid operated valves that can be mounted on a single aluminum subbase, or manifolds up to 16 stations. Components can be ordered separately, or custom made, factory assembled and tested manifold assemblies are available. Standard voltages are 12VDC and 24 VDC in 2/2 normally closed, and 3/2 normally open or closed configurations. Other voltages and many other options are available upon request, including customized manifolds with integrated wiring to a multi-pin connector, and special higher flow versions. Both valve series are interchangeable with several other manufacturers’ 10mm and 15mm valves, and are very economically priced.

The 10mm DO10-MR valve comes standard with a push type manual override with a working pressure is 0 to 102 psi. Standard electrical connections include 300mm flying leads and a 2-pin 90° connection with LED. The DO10-MR features fast response times of 8 ms when energized, and 10 ms when de-energized. Optional configurations are available upon request.

The 15mm DO15-MR valve comes standard with a push type non-locking or a two-position locking manual override. Working pressure is 0 to 73 psi for the normally open versions, and 0 to 102 psi for the normally closed versions. Standard electrical connections include 300mm flying leads, a 2-pin 90° connection with LED, and a DIN Form C. The DO15-MR features fast response times of 10 ms when energized, and 12 ms when de-energized. Optional configurations are available upon request.

Visit Bosch Rexroth at AATExpo 2011 in Chicago’s McCormick Place, booth 1308. For more information, please visit www.boschrexroth-us.com/brp.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue ($6.8 billion) in 2010. To learn more, please visit www.boschrexroth-us.com.

The Bosch Group is a leading global supplier of technology and services. In the areas of automotive and industrial technology, consumer goods, and building technology, some 285,000 associates generated sales of 47.3 billion euros ($62.7 billion) in fiscal 2010. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in over 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent 3.8 billion euros for research and development in 2010, and applied for over 3,800 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Additional information can be accessed at www.bosch.com , www.bosch-press.com.

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com