xxx 2011-09-20

AATExpo 2011: trCD04 Pneumatic Directional Control Valves

AATExpo 2011: trCD04 Pneumatic Directional Control Valves

Rexroth Series CD04 inch version valves provide a highly reliable, high flow, cost effective solution to a wide variety of applications.

Bosch Rexroth has expanded the Series CD04 valve line to include inch porting in addition to ISO-G (BSPP) porting.

(Lexington, KY – With a width of only 26 millimeters, the universally applicable CD04 inch version valves provide a high 0.9Cv flow rate. A combination of electrically actuated, pneumatically actuated, and manually/mechanically actuated valves offers the user flexibility.

The die-cast zinc polyamide/fiberglass reinforced body results in a durable yet light-weight package. The CD04 Inch series features a standard Form B electrical connection, choice of 1/8” PTF (NPT short threads) or ISO-G1/8 (BSPP) ports, and they can even be used for vacuum or dual pressure applications.

Other features include:

  • 3-way 2-position, 5-way 2-position, and 5-way 3-position spool options
  • Electrical voltages 12 VDC, 24 VDC, and 110 VAC, or basic valves without coil for other voltages
  • Single and double air pilot versions
  • Manual/Mechanical options for plunger, pushbutton, lever, and roller actuators

Visit Bosch Rexroth at AATExpo 2011 in Chicago’s McCormick Place, booth 1308. For more information, please visit

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 34,900 associates generated approximately 5.1 billion euros in revenue ($6.8 billion) in 2010. To learn more, please visit

The Bosch Group is a leading global supplier of technology and services. In the areas of automotive and industrial technology, consumer goods, and building technology, some 285,000 associates generated sales of 47.3 billion euros ($62.7 billion) in fiscal 2010. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in over 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent 3.8 billion euros for research and development in 2010, and applied for over 3,800 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Additional information can be accessed at ,


Search press releases


Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670