USA

Select your location

USA
 

Press

Content
xxx 2011-02-08

trCD04 Pneumatic Directional Control Valves

trCD04 Pneumatic Directional Control Valves

Rexroth Series CD04 inch version valves provide a highly reliable, high flow, cost effective solution to a wide variety of applications.

(Lexington, KY – www.boschrexroth-us.com) With a width of only 26 millimeters, the universally applicable CD04 inch version valves provide a high 0.9Cv flow rate. A combination of electrically actuated, pneumatically actuated, and manually/mechanically actuated valves offers the user flexibility.

The die-cast zinc polyamide/fiberglass reinforced body results in a durable yet light-weight package. The CD04 Inch series features a standard Form B electrical connection, choice of 1/8” PTF (NPT short threads) or ISO-G1/8 (BSPP) ports, and they can even be used for vacuum or dual pressure applications.

Other features include:

  • 3-way 2-position, 5-way 2-position, and 5-way 3-position spool options
  • Electrical voltages 12 VDC, 24 VDC, and 110 VAC, or basic valves without coil for other voltages
  • Single and double air pilot versions
  • Manual/Mechanical options for plunger, pushbutton, lever, and roller actuators

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 38,400 associates generated approximately 6.4 billion euros in revenue in 2011.

To learn more, please visit www.boschrexroth-us.com

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software innnovations. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011, per preliminary figures. For more information, visit www.boschusa.com.

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Further information is available online at www.bosch.com and www.bosch-press.com.

 

Search press releases


Contact

John  Bridges
Mercer Road 1653
40511 Lexington, KY
Phone: (859) 281-3417
Fax: (859) 281-3491
john.bridges@boschrexroth-us.com