USA

Select your location

USA
 

Press

Content
xxx 2011-02-08

Miniature 10mm and 15mm Pneumatic Valves

Miniature 10mm and 15mm Pneumatic Valves

The modular line of 3/2 and 2/2 miniature direct-acting valves with 10mm and 15mm valve body widths feature fast response, with a high flow rate, at an economical price.

(Lexington, KY – www.boschrexroth-us.com) The DO10-BR and DO15-BR are direct-acting, solenoid operated valves that can be mounted on a single aluminum subbase, or manifolds up to 16 stations. Components can be ordered separately, or custom made, factory assembled and tested manifold assemblies are available. Standard voltages are 12VDC and 24 VDC in 2/2 normally closed, and 3/2 normally open or closed configurations. Other voltages and many other options are available upon request, including customized manifolds with integrated wiring to a multi-pin connector, and special higher flow versions. Both valve series are interchangeable with several other manufacturers’ 10mm and 15mm valves, and are very economically priced.

The 10mm DO10-BR valve comes standard with a push type manual override with a working pressure is 0 to 102 psi. Standard electrical connections include 300mm flying leads and a 2-pin 90° connection with LED. The DO10-BR features fast response times of 8 ms when energized, and 10 ms when de-energized. Optional configurations are available upon request.

The 15mm DO15-BR valve comes standard with a push type non-locking or a two-position locking manual override. Working pressure is 0 to 73 psi for the normally open versions, and 0 to 102 psi for the normally closed versions. Standard electrical connections include 300mm flying leads, a 2-pin 90° connection with LED, and a DIN Form C. The DO15-BR features fast response times of 10 ms when energized, and 12 ms when de-energized. Optional configurations are available upon request.

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 38,400 associates generated approximately 6.4 billion euros in revenue in 2011.

To learn more, please visit www.boschrexroth-us.com

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software innnovations. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011, per preliminary figures. For more information, visit www.boschusa.com.

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Further information is available online at www.bosch.com and www.bosch-press.com.

 

Search press releases


Contact

John  Bridges
Mercer Road 1653
40511 Lexington, KY
Phone: (859) 281-3417
Fax: (859) 281-3491
john.bridges@boschrexroth-us.com