USA

Select your location

USA
 

Press

Content
xxx 2012-11-20

Rexroth IndraMotion MTX the first CNC certified for the Sercos automation bus

The IndraMotion MTX performance CNC, using the CML 65 controller, has recently been certified as a product that conforms to the Ethernet standard Sercos the automation bus. This certification makes the Rexroth IndraMotion MTX CNC the first CNC controller available to receive this certification. What makes this CNC controller unique is not just the performance and scalability of the controller but the combination of speed, tight motion / IO synchronization performance and flexibility of Sercos the automation bus. With both technologies blended into one system, the optimal performance can be achieved for a wide range of CNC applications. Be it traditional metal cutting, 5-axis die and mold, punching, bending, laser, water jet, plasma, assembly and automation – Sercos for I/O and electric or hydraulic motion ensures the highest productivity.

The Sercos automation bus enables the simple integration of many other Rexroth technologies such as electric and hydraulic servo motion, digital & analog I/O and pneumatics all tightly synchronized with the interpolation update rate on a single automation bus. Due to the standard Ethernet conformance, Sercos is compatible to any Ethernet-based protocol and shares the Ethernet media in the friendliest way.

Customers use Rexroth’s wide range of Sercos products to build extremely productive and innovative machinery which is in high demand today and in the future. Rexroth products that use Sercos the automation bus:

Control systems:

  • IndraMotion MTX – CNC system with up to 64 axes
  • IndraMotion MLC – Motion Logic system with digital axis synchronization
  • IndraMotion MLD – Drive based motion and logic control
  • IndraLogic XLC – Fast IEC61131-3 PLC w/ motion control

I/O:

  • Inline Sercos I/O - Rail mounted modular I/O
  • Inline compact I/O – Analog, digital, standard, fast and 4-axes module
  • IndraControl S20 – Low profile high-speed I/O
  • IndraControl S67 – IP67 fixture mount I/O

Electric Drives:

  • IndraDrive – 100 W to 630 kW
  • IndraDrive Mi – motor integrated IndraDrive

Hydraulic motion:

  • HNC 100-3x – Hydraulic servo valve controller
  • IACR-2x – Hydraulic servo valve with integrated controller

Pneumatics:

  • BDC-B – Pneumatic valve HF03/HF04 manifold interface

Tightening:

  • CS351 – Controller for Rexroth electric nutrunner

Welding:

  • PSI63C0 - Inverter up to 36 kA for perfect resistance welding

The convenience of Sercos the automation bus has made it possible to quickly integrate many other high performance third party offerings - see www.sercos.de/en

Bosch Rexroth AG is one of the world’s leading specialists in the field of drive and control technologies. Under the Rexroth brand name, the company supplies more than 500,000 customers with tailored solutions for driving, controlling, and moving. Bosch Rexroth is a partner for Mobile Applications, Machinery Applications and Engineering, Factory Automation and Renewable Energies. The company provides customized solutions tailored to the needs and specifications of each individual market. As The Drive & Control Company, Bosch Rexroth develops, produces, and sells components and systems in over 80 countries. As part of the Bosch Group, Bosch Rexroth and its 38,400 associates generated approximately 6.4 billion euros ($8.9 billion) in revenue in 2011.

To learn more, please visit ww.boschrexroth-us.com.

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software innovations. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011, per preliminary figures. For more information, visit www.boschusa.com.

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Further information is available online at www.bosch.com and www.bosch-press.com.

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com