USA

Select your location

USA
 

Press

Content
xxx 2012-09-06

IMTS 2012: IndraMotion MTX CNC solution enhances productivity in machine tools

IMTS 2012: IndraMotion MTX CNC solution enhances productivity in machine tools

Equipped with a multi-core processor, the IndraMotion MTX CNC platform executes programs at top speed, boosting machine productivity

Enhancing productivity while reducing energy consumption – it’s not a contradiction in terms. The IndraMotion MTX CNC solution from Rexroth helps machine manufacturers and operators to balance these two key requirements and achieve both in optimum style. To do so, the drive and control specialist Rexroth has introduced a number of innovations in the hardware and software used for the system. CML 85 control hardware equipped with a multi-core processor execute programs at top speed, boosting productivity. The energy monitoring function of the software records energy consumption, either by specific consumers such as drive axes or by work piece, facilitating energy efficiency in machine tool operation.

The IndraMotion MTX CNC solution with integrated IEC 61131 PLC is scalable in terms of functionality and productivity: Depending on the number of axes, users can choose between the variants micro, standard, performance, and advanced.

The IndraMotion MTX advanced CNC, using CML 85 multi-core processor hardware, was designed especially for machines with many axes and complex production processes that utilize multiple production technologies in a single work piece clamping. Intelligent distribution of control sequences to the multi-core processor architecture delivers the added performance necessary to execute programs even faster. The control system reaches a CNC interpolation time that ranges from 0.25 ms to 1 ms, which decreases auxiliary process times and enhances productivity.

Energy monitoring makes consumption transparent

With the energy monitoring function, operators can document the energy consumption of individual consumers such as drive axes or ancillary units for hydraulics and cooling lubricants, but it is also possible to determine energy consumption per work piece. When changes are made to the work piece material, when the tools show wear and tear, or when the auxiliary substances or lubricants are changed, this feature then allows for comparisons based on trending diagrams, making energy consumption transparent. Intelligent standby functions also make it possible to successively shut down those parts that require the most energy, for example until raw parts are available again.

Universal ‘run from’ function and new processing cycles

When large machining programs are interrupted, it is important to operators to ensure that processing can be continued precisely from where it was interrupted. The new universal ‘run from’ function of the IndraMotion MTX allows just that, by guiding the operator through the restart of the processing program. Detailed diagnoses show the machine operator where it is necessary to adjust the current machine status to the target status that is necessary to continue the program.

New processing cycles for milling allow operators to determine, based on simple criteria, whether the focus should be the processing time or the processing quality of a work piece. The rough machining of a work piece can thus be done very quickly, while the machine tool performs the subsequent precision machining with greater precision.

The latest version of IndraMotion MTX CNC is equipped with an Ethernet field bus interface for multi-protocol operation, so manufacturers can choose between PROFINET and Ethernet/IP. Depending on the specific system configuration, Sercos, PROFIBUS, PROFINET, or Ethernet/IP can simply be configured in software to exchange data on the sensor-actuator level. The communication with the drive level is carried out via Sercos interface with Ethernet; the major advantage of this approach is that users can control electrical and hydraulic motion with I/O and pneumatics, tightly synchronized with the interpolation update rate on a single bus.

For a list of specifications as well as available features and accessories please visit www.boschrexroth-us.com.

In the U.S., Canada and Mexico, the Bosch Group manufactures and markets automotive original equipment and aftermarket products, industrial drives and control technology, power tools, security and communication systems, packaging technology, thermotechnology, household appliances, solar energy, healthcare telemedicine and software innovations. Having established a regional presence in 1906, Bosch employs over 22,500 associates in more than 100 locations, with sales of $9.8 billion in fiscal year 2011, per preliminary figures. For more information, visit www.boschusa.com.

The Bosch Group is a leading global supplier of technology and services. According to preliminary figures, more than 300,000 associates generated sales of 51.4 billion euros ($71.5 billion) in the areas of automotive and industrial technology, consumer goods, and building technology in fiscal year 2011. The Bosch Group comprises Robert Bosch GmbH and its more than 350 subsidiaries and regional companies in some 60 countries. If its sales and service partners are included, then Bosch is represented in roughly 150 countries. This worldwide development, manufacturing, and sales network is the foundation for further growth. Bosch spent more than 4 billion euros ($5.5 billion) for research and development in 2011, and applied for over 4,100 patents worldwide. With all its products and services, Bosch enhances the quality of life by providing solutions which are both innovative and beneficial. Further information is available online at www.bosch.com and www.bosch-press.com.

 

Search press releases


Contact

Susan  Strauss
City Line Road 2315
18017 Bethlehem, PA
Phone: (610) 694-8352
Fax: (610) 954-8670
susan.strauss@boschrexroth-us.com